STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

problem with own machine. DDR error

Hello I created own machine based of seeed module. at the strartup there is info NOTICE: CPU: STM32MP157CAC Rev.B   NOTICE: Model: STMicroelectronics custom STM32CubeMX board - openstlinux-5.10-dunfell-mp1-21-03-31   WARNING: VDD unknown   INFO: Res...

TStas.2 by Associate II
  • 1425 Views
  • 4 replies
  • 0 kudos

Resolved! android on stm32mp157c-dk2

Hi Nicolas L (ST Employee),I have read the past article that you provide sources and directives to allow building the Android 10 delivery for the STM32MP157C-DK2.Could you please send me the solution?I hope you will be able to reply to me.By the way,...

HiroM by Associate II
  • 1379 Views
  • 4 replies
  • 0 kudos

i2c2

I'm working with the DevBoard from Myir MYD-YA-157C which has the stm32mp157 MPU. I'm trying to chech the i2c from the M4 in the Engineering mode and have a problem.When I tied the I2C_TwoBoards_ComIT, it works. At least it generates the I2C5_ER_IRQ....

How do I fix "undefined reference to `OPENAMP_create_endpoint'" within the OpenAmp source.

I've added OPENAMP through the middleware after enableing the IPCC interrupts, but now I'm getting the following error and an error in the actual OPENAMP source that's included!/opt/st/stm32cubeide_1.8.0/plugins/com.st.stm32cube.ide.mcu.externaltools...

msche.1 by Associate III
  • 1232 Views
  • 1 replies
  • 0 kudos