STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP1 OpenAMP IPC

I was looking into using OpenAMP to support an event driven IPC between Linux A7 core and a FreeRTOS based application running on the M4. The sample application (STM32CubeMP15 Firmware Package )documentation in the says:"The actual bare metal version...

Dowlers by Associate
  • 855 Views
  • 0 replies
  • 0 kudos

Hi: I use ecosystem 4.0. When I write a program to stm32mp157 through stmcubeprogrammer, the following problems occur: Error: an error occured while uploading data from the virtual partition 0xF1

the ssh print:U-Boot 2021.10-stm32mp-r1 (Jul 20 2022 - 10:52:56 +0800)CPU: STM32MP157DAA Rev.ZModel: STMicroelectronics STM32MP157D eval daughterBoard: stm32mp1 in trusted - stm32image mode (st,stm32mp157d-ed1)DRAM: 1 GiBClocks:- MPU : 650 MHz- MCU :...

zxiao.4 by Associate III
  • 995 Views
  • 4 replies
  • 0 kudos

Resolved! Project building process

Hy there!I'm new on ST platforms and development environments (I'm used to Netbeans-like ones).Well, I would like to copy (automatically) both .elf executable and the .map files in given folder after building the projet.This folder ("Out") is placed ...

iTTy by Senior
  • 1576 Views
  • 4 replies
  • 0 kudos

Resolved! libdbus-1-3 (>= 1.12.20)

My package is http://packages.openstlinux.st.com/3.1 ,I cannot update cups.When I install cups,the "cups : Depends: libdbus-1-3 (>= 1.12.20) but 1.12.16-r0.1 is to be installed" appeared,How can I install the libdbus-1-3 (>= 1.12.20) ? Thanks.

zxiao.4 by Associate III
  • 1018 Views
  • 6 replies
  • 0 kudos

Resolved! How do I build and boot ATF and OP-TEE?

Hi! It's my understanding that ST are moving a lot of work for power management and clocking out of ATF and to OP-TEE. In preparation for this shift my co-developer and I have started out trying to build and run the following software on the STM32MP1...

JGuy1 by Associate II
  • 2305 Views
  • 3 replies
  • 0 kudos