2021-06-28 9:16 PM
I want to store some configurations in the OTP. The datasheet states that the OTP word 59 to 95 are free for users. In DK boards, OTP word 59 is already claimed as board_id, so I use word 60 as my starting point. Currently, I am using both environments 3.0 (using yocto) and 2.0 (using buildroot) and I prepared the OTP map by modifying the tf-a device tree.
---------------------------------------------
&bsec{
status = "okay";
secure-status = "okay";
board_id: board_id@ec {
reg = <0xec 0x4>;
st,non-secure-otp;
};
conf_sec: conf_sec@f0 {
reg = <0xf0 0x40>;
st,non-secure-otp;
};
};
---------------------------------------------
&nvmem_layout {
nvmem-cells = <&cfg0_otp>,
<&part_number_otp>,
<&monotonic_otp>,
<&nand_otp>,
<&uid_otp>,
<&package_otp>,
<&hw2_otp>,
<&pkh_otp>,
<&board_id>,
<&conf_sec>;
nvmem-cell-names = "cfg0_otp",
"part_number_otp",
"monotonic_otp",
"nand_otp",
"uid_otp",
"package_otp",
"hw2_otp",
"pkh_otp",
"board_id",
"conf_sec";
};at first, I successfully flashed the image and write the OTP to word 60. However, I cannot read the OTP table after I write my configuration to the OTP
after I got the error, I thought that I only need to reboot the board. But unfortunately, the board failed to boot. I tried to re-flash the image but the I got a timeout error. The serial out showed something like this.
After I tried with multiple boards, I found out that I can only write the lower 16-bit of the OTP word (ex, 0x0000FFFF). However, if I change any single bit in the upper 16-bit of the OTP word, the board will break.
I believe there is something wrong with OTP mapping that makes the image failed to boot from MMC or USB/Serial. Now, I need help to resolve this issue because I have 3 broken DK boards
2021-06-30 4:21 AM
Hi @jandriea ,
Not clear if you are still able to boot up to Uboot ?
If yes can you please send the boot log and try to read the OTP from Uboot ?
https://wiki.st.com/stm32mpu/wiki/How_to_update_OTP_with_U-Boot
Thanks
Olivier
2021-07-12 12:17 AM
Hi @Community member
Unfortunately, the boards are unable to boot up to uboot. The boot sequence stopped after printing these messages
========================
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0x2ffeb000
INFO: SPSR = 0x1d3
=======================
2022-07-13 10:35 PM
The same problem. It is not possible to write to user space in otp? How to fix broken boards?