STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STUSB1600 (USB-C) Alternatives

Hey,I am designing a board based on the STM32MP157F using the OSD32MP157F SOM as a base. I want to have a usb-c connector acting as a host and/or as hs_otg. Reviewing the DK boards schematics I see that the STUSB1600 is being used. I also see on the ...

Sindel by Associate
  • 1241 Views
  • 0 replies
  • 0 kudos

Resolved! STM32MP15x ADC Oversample

Could someone point me to some documentation about how to control the oversampling for ADC1 and ADC2 for the STM32MP157C?    Using OpenSTLinux 4.1.0, buildroot.   I looked around but couldn't find anything. Thanks!

Macdog by Associate III
  • 1834 Views
  • 1 replies
  • 0 kudos

Switch uboot logs to usart6

Hello, I have a board based on the stm32mp153a and I'm trying to get it to boot, unfortunately I can only access USART 6 while it seems that uboot only tries to interact using uart4.In my dbs file I have overridden usart6/status to be "okay" instead ...

STM32MP1 I2S_CKIN as source for PLL4

Hi there,in order to have an externally generated clock for our LTDC peripheral we decided to use the I2S_CKIN as the reference clock for PLL4 on our customized STM32MP157CAC board. Reference manual and STM32CubeMX are showing that this opportunity e...

HAL9000 by Associate
  • 1196 Views
  • 0 replies
  • 1 kudos

Resolved! stm32mp135 PA10 as tim1 ch3 pwm

Hi,I have a problem with the configuration of PA10 of stm32mp135 to work as pwm of TIM1_CH3. I also make an experiment to disable completely timer and PWM and I also can't control this pin using gpioset. In the documentation I saw that this pin is de...

MWoło.2 by Senior III
  • 2427 Views
  • 7 replies
  • 0 kudos

Resolved! libqmi build for STM32MP157

I'm building libqmi for the STM32MP157 and getting an error  at this point in the build GISCAN Qmi-1.0.girTraceback (most recent call last):File "/home/ed/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-v...

edwardmcl by Associate II
  • 1947 Views
  • 2 replies
  • 0 kudos