cancel
Showing results for 
Search instead for 
Did you mean: 

Power supply for STM32MP157D-DK1-ND development kit specifies 5V/3A. However, can we use fast charger for the same? Specs for the fast charger: 5V/3A , 9V/2.77A (PPS 25W). Will the fast charger supply a 9V/2.77A input instead of 5V/3A. Any suggestions?

VUnni.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
PatrickF
ST Employee

Hi @VUnni.1​ 

to complete the answer from @Kevin HUBER​ , any "USB Type-C compliant" supply rated above 5V/3A will work.

Supply rated 5V/3A , 9V/2.77A (or above) will work as well. Per USB standard, supply must start with a default 5V when pull-down on CC line is detected. The 9V or above voltage will be enabled only after successful 'power delivery' negotiation (which obviously is not done by STM32MP157x-DKx boards).

Even if rated 5V/3A, supply with Type-A socket with a Type-A <-> Type-C cable are usually showing warning (blinking led) but could work (but sometimes not recognized and uboot will stop).

This (old) post could help you.

https://community.st.com/s/question/0D50X0000Bftr1ySQA/power-supply-for-stm32mp157cdk2

Regards.

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

View solution in original post

2 REPLIES 2
Kevin HUBER
ST Employee

Hello @VUnni.1​ ,

If you look at the user manual of your board page 10:

https://www.st.com/resource/en/user_manual/dm00652742-.pdf

It is recommended to
use a USB Type-C® to USB Type-C® 5 V/3 A charger.

Otherwise, we can't guarantee whether it will work or not.

Best Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
NEW ! Sidekick STM32 AI agent, see here
PatrickF
ST Employee

Hi @VUnni.1​ 

to complete the answer from @Kevin HUBER​ , any "USB Type-C compliant" supply rated above 5V/3A will work.

Supply rated 5V/3A , 9V/2.77A (or above) will work as well. Per USB standard, supply must start with a default 5V when pull-down on CC line is detected. The 9V or above voltage will be enabled only after successful 'power delivery' negotiation (which obviously is not done by STM32MP157x-DKx boards).

Even if rated 5V/3A, supply with Type-A socket with a Type-A <-> Type-C cable are usually showing warning (blinking led) but could work (but sometimes not recognized and uboot will stop).

This (old) post could help you.

https://community.st.com/s/question/0D50X0000Bftr1ySQA/power-supply-for-stm32mp157cdk2

Regards.

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here