STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP135F-DK How to set LDO2

Hi, I have an STM32MP135F-DK board, and I want to set LDO2 and get an output voltage of 3.3V. I have read a document ( Integration of STM32MP13x MPU product lines and STPMIC1D / STPMIC1A on a wall adapter supply) which states that LDO2 must be set af...

gunesalp by Associate
  • 3389 Views
  • 1 replies
  • 0 kudos

Drive DSI data lanes to LP-11

Hello. I need to integrate a TI SN65DSI83 bridge with a DK2 board and one of the requirements of that bridge is to drive the data lanes to LP-11 state. What is the procedure to make that happen? I am assuming I need to make changes to dw-mipi-dsi / d...

EMaes.1 by Associate II
  • 2406 Views
  • 3 replies
  • 0 kudos

Resolved! STM32MP135 PANIC and DDR frequency error

Hello ST community,I am designing a board with STM32MP135 CPU and DDR3L based from STM32MP135F-DK.DDR stress test passed successfully and tf-a files are adjusted to have I2C4 on pins used in my design (SCL on PB13 and SDA on PB7).When I flash board t...

Vince60_0-1694011522130.png Vince60_1-1694011539770.png
Vince60 by Associate II
  • 5324 Views
  • 4 replies
  • 1 kudos

Resolved! Black screen when enabling galcore

Many thanks for your help!I have a custom STM32MP157c boards that works OK when the galcore.ko module is not deployed.When the galcore,ko module is deployed, the screen doesn't show up the usual image and after the boot image has been displayed, it s...

STM32MP1 pixel format RGB666

Hello,according to drivers/gpu/drm/stm/ltdc.c stm hardware supports these pixel formats:enum ltdc_pix_fmt {PF_NONE,/* RGB formats */PF_ARGB8888, /* ARGB [32 bits] */PF_RGBA8888, /* RGBA [32 bits] */PF_RGB888, /* RGB [24 bits] */PF_RGB565, /* RGB [16 ...

mishuk by Associate III
  • 2875 Views
  • 2 replies
  • 0 kudos

Murata 1DX driver issue

Hello all,We have a custom board with STM32MP157FAC1.Kernel version is 5.10.153.I know that Murata 1DX is used on STM32MP157C-DK2 board and that's why we choose it to use in our product.But in our case, module is waiting in loading state.The command ...