STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Getting error/warning "Gtk-WARNING **: 18:09:46.325: cannot open display:" while executing "hello-world" sample application with STM32MP157F-DK2. Expected a GTK window is NOT displayed on display screen

Hi, I'm getting error "(gtk_hello_world:1474): Gtk-WARNING **: 18:09:46.325: cannot open display: " while executing "hello-world" sample application with STM32MP157F-DK2. Expected a GTK window is NOT displayed on display screenI have followed steps a...

S.Kamath by Associate III
  • 3802 Views
  • 2 replies
  • 0 kudos

STM32MP15 OPTEE Minimum DDR3

Hello,I am having trouble booting OPTEE on a custom platform with 256MB of DDR3. The boot log is attached. I added some debug printfs and I can see that OPTEE freezes on 454 in core/arch/arm/kernel/boot.c. I believe this is the first time OPTEE start...

Resolved! Setting SPI clock to 20 MHz and beyond

Hello,my system is based on an STM32MP151x, running embedded Linux (Buildroot generated + all the ST patches, v5.3.56). I am suing an SPI connection to an external hardware but so far, i am not able to set the SPI clock to 20MHz and higher.Looking at...

JSamo.2 by Associate II
  • 1894 Views
  • 3 replies
  • 0 kudos