cancel
Showing results for 
Search instead for 
Did you mean: 

How to get STM32MP157F-DK2 starter package with latest GLIBC 2.35?

S.Kamath
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
OlivierK
ST Employee

Hi S.Kamath (Community Member)

On OSTL DV4.1, natively I have libc 2.35 using the starter package.

libc6 is already the newest version (2.35-r0).

If you use an old OSTL version, the starter image supports debian package update/install.

Just plug the ethernet cable or configure the wifi connected to the net.

root@stm32mp1:~# apt-get install libc

Regards,

Olivier


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
OlivierK
ST Employee

Hi S.Kamath (Community Member)

On OSTL DV4.1, natively I have libc 2.35 using the starter package.

libc6 is already the newest version (2.35-r0).

If you use an old OSTL version, the starter image supports debian package update/install.

Just plug the ethernet cable or configure the wifi connected to the net.

root@stm32mp1:~# apt-get install libc

Regards,

Olivier


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
S.Kamath
Associate III

Thanks Olivier,

I noticed today that discovery kit was not flashed properly with new OSTL DV4.1 when I tried to flash earlier from a Linux system. So, default OSTL version was there in the discovery kit. I successfully flashed latest OSTL DV4.1 today from Windows desktop today.