STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I2C in STM32MP13xx giving continuously NACK after start condition with STPMIC1 in bare-metal environment

Hi,I am working on STM32MP133FAFx (I2C Master) for I2C communication with STPMIC1 IC (I2C slave) fast mode(400KHz) and HSI clock(64MHz). I2C->TIMINGR = 0x00C0216CI am trying polling method in bare-metal environment for communication in I2C.Below is m...

2 Host and 1 device USB

My current application uses 2 USB ports, both connected to USBPHYC (STM32MP157F). The OTG one is used for programming using CubeProgrammer.My new revision requires 3 USB ports, 2 host and the programming port.According to https://community.st.com/t5/...

allard by Senior
  • 1540 Views
  • 1 replies
  • 0 kudos

Connecting 2 codecs on MP257

I am trying to connect to audio codecs to give 4 channel of audio on a MP257. Can I connect SAI2.SCKA TO BCK on both , SAI2.FSA to LRCK on both, SAI2.SDA to DIN on the first and SAI2.SDB to DIN on the second.My concern is the clocking, can I common b...

Schematic of 2 codecs.png RM 81.4.3.png
SCROGGYG by Associate II
  • 1153 Views
  • 0 replies
  • 0 kudos