STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP1 DDR Routing Rules

I entered the lengths of the DDR traces from the ST official evaluation board into Excel, and the maximum length deviation is 3 mm. Is the trace routing on the evaluation board reasonable, and can I reuse it directly on my own board?   

LH1 by Associate II
  • 329 Views
  • 3 replies
  • 0 kudos

Bug/Issue in helper scripts

Following the tutorial here, when I get to the step "To generate binary to flashing via Cortex-A", the helper script fails to build when given the 'programmer' argument.  The problem appears to be incorrect configuration of the path to a device tree ...

ADunc.1 by Senior II
  • 195 Views
  • 0 replies
  • 0 kudos

Resolved! STM32MP1 boot from EMMC

Hello everyone,I have a custom board based on STM32MP157A (rev. Z) and I am trying to boot from emmc; I am able to boot sucessfully from SD card; I flashed the same image to the emmc with the ST MX Cube Programmer and, if get into u-boot from SD card...

bimorqt by Associate III
  • 5889 Views
  • 3 replies
  • 1 kudos