cancel
Showing results for 
Search instead for 
Did you mean: 

Bug/Issue in helper scripts

ADunc.1
Senior II

Following the tutorial here, when I get to the step "To generate binary to flashing via Cortex-A", the helper script fails to build when given the 'programmer' argument.  The problem appears to be incorrect configuration of the path to a device tree file.  

All other steps in the tutorial build correctly using the device tree files given, just not the programmer step fails.

The output is shown below.  In it you can see the following paths are supplied:

EXTDT_DIR=/home/ashley/STM32MPU-Ecosystem-v6.2.0/Developer-Package/stm32mp2-openstlinux-26.02.18/sources/STM32MP215DK-AshMX
EXTDT_DIR_OPTEE=CA35/DeviceTree/STM32MP215DK-AshMX/optee-os

The correct path to the dts file is ${EXT_DIR}/${EXTDIR_DIR_OPTEE}, but the path actually searched for the dts file is (refer line 58 in the log below):

/home/ashley/STM32MPU-Ecosystem-v6.2.0/Developer-Package/stm32mp2-openstlinux-26.02.18/sources/STM32MP215DK-AshMX/stm32mp2/a35-td/optee/

Full log is:

sdk_compilation-stm32mp2-mx-my-custom-board.sh programmer

Your configuration:
     sdk_absolute_path                 = /home/ashley/STM32MPU-Ecosystem-v6.2.0/Developer-Package/SDK
     sdk_env_file                      = environment-setup-cortexa35-ostl-linux
     your_board_name                   = stm32mp215f-stm32mp215dk-ashmx-mx
     your_soc_name                     = stm32mp21
     your_storage_boot_scheme_security = optee
     your_storage_boot_scheme_cortex_a = optee-sdcard
     your_deploy_dir_path              = /home/ashley/STM32MPU-Ecosystem-v6.2.0/Developer-Package/stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18/sources/ostl-linux/output-sdk-stm32mp215fdk-ash
     your_build_subdir_path            = ../build
     your_cubemx_project_name          = STM32MP215DK-AshMX
     externaldt_path                   = /home/ashley/STM32MPU-Ecosystem-v6.2.0/Developer-Package/stm32mp2-openstlinux-26.02.18/sources/STM32MP215DK-AshMX

**** stm32mp-ddr-phy_set ****START****
[CMD]:>  cd stm32mp-ddr-phy-A2022.11-r0
[CMD]:>  cd stm32mp-ddr-phy-A2022.11
[CMD]:>  cd ..
[CMD]:>  export FWDDR_DIR=/home/ashley/STM32MPU-Ecosystem-v6.2.0/Developer-Package/stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18/sources/ostl-linux/stm32mp-ddr-phy-A2022.11-r0/stm32mp-ddr-phy-A2022.11
**** stm32mp-ddr-phy_set ****END****
**** external-dt_set ****START****
[CMD]:>  cd external-dt-v6.0-stm32mp-r3-r0
[CMD]:>  cd external-dt-v6.0-stm32mp-r3
**** external-dt_set ****END****
**** optee-os-stm32mp_set ****START****
[CMD]:>  cd optee-os-stm32mp-4.0.0-stm32mp-r3-r0
[CMD]:>  cd optee-os-stm32mp-4.0.0-stm32mp-r3
[CMD]:>  export FIP_DEPLOYDIR_ROOT=/home/ashley/STM32MPU-Ecosystem-v6.2.0/Developer-Package/stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18/sources/ostl-linux/output-sdk-stm32mp215fdk-ash
**** optee-os-stm32mp_set ****END****
**** u-boot-stm32mp_set ****START****
[CMD]:>  cd u-boot-stm32mp-v2023.10-stm32mp-r3-r0
[CMD]:>  cd u-boot-stm32mp-v2023.10-stm32mp-r3
[CMD]:>  export FIP_DEPLOYDIR_ROOT=/home/ashley/STM32MPU-Ecosystem-v6.2.0/Developer-Package/stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18/sources/ostl-linux/output-sdk-stm32mp215fdk-ash
**** u-boot-stm32mp_set ****END****
**** tf-a-stm32mp_set ****START****
[CMD]:>  cd tf-a-stm32mp-v2.10.24-stm32mp-r3-r0
[CMD]:>  cd tf-a-stm32mp-v2.10.24-stm32mp-r3
[CMD]:>  export FIP_DEPLOYDIR_ROOT=/home/ashley/STM32MPU-Ecosystem-v6.2.0/Developer-Package/stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18/sources/ostl-linux/output-sdk-stm32mp215fdk-ash
**** tf-a-stm32mp_set ****END****
**** linux-stm32mp_set ****START****
[CMD]:>  cd linux-stm32mp-6.6.116-stm32mp-r3-r0
[CMD]:>  cd linux-6.6.116
[CMD]:>  export KERNEL_BUILDDIR=/home/ashley/STM32MPU-Ecosystem-v6.2.0/Developer-Package/stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18/sources/ostl-linux/linux-stm32mp-6.6.116-stm32mp-r3-r0/build
**** linux-stm32mp_set ****END****
**** gcnano-driver-stm32mp_set ****START****
**** gcnano-driver-stm32mp_set ****END****
**** stm32mp-ddr-phy_programmer_compile ****START****
**** stm32mp-ddr-phy_programmer_compile ****END****
**** external-dt_programmer_compile ****START****
**** external-dt_programmer_compile ****END****
**** optee-os-stm32mp_programmer_compile ****START****
[CMD]:>  cd optee-os-stm32mp-4.0.0-stm32mp-r3-r0
[CMD]:>  cd optee-os-stm32mp-4.0.0-stm32mp-r3
[CMD]:> export BLD_PATH=/home/ashley/STM32MPU-Ecosystem-v6.2.0/Developer-Package/stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18/sources/ostl-linux/optee-os-stm32mp-4.0.0-stm32mp-r3-r0/build-programmer
[CMD]:>  make -f /home/ashley/STM32MPU-Ecosystem-v6.2.0/Developer-Package/stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18/sources/ostl-linux/optee-os-stm32mp-4.0.0-stm32mp-r3-r0/optee-os-stm32mp-4.0.0-stm32mp-r3/../Makefile.sdk.stm32mp2 OPTEE_CONFIG=optee-programmer CFG_EMBED_DTB_SOURCE_FILE=stm32mp215f-stm32mp215dk-ashmx-mx DEPLOYDIR=/home/ashley/STM32MPU-Ecosystem-v6.2.0/Developer-Package/stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18/sources/ostl-linux/output-sdk-stm32mp215fdk-ash/optee EXTDT_DIR=/home/ashley/STM32MPU-Ecosystem-v6.2.0/Developer-Package/stm32mp2-openstlinux-26.02.18/sources/STM32MP215DK-AshMX EXTDT_DIR_OPTEE=CA35/DeviceTree/STM32MP215DK-AshMX/optee-os  optee
make[1]: Entering directory '/home/ashley/STM32MPU-Ecosystem-v6.2.0/Developer-Package/stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18/sources/ostl-linux/optee-os-stm32mp-4.0.0-stm32mp-r3-r0/optee-os-stm32mp-4.0.0-stm32mp-r3'
core/arch/arm/plat-stm32mp2/conf.mk:25: *** Cannot find DTS file /home/ashley/STM32MPU-Ecosystem-v6.2.0/Developer-Package/stm32mp2-openstlinux-26.02.18/sources/STM32MP215DK-AshMX/stm32mp2/a35-td/optee/stm32mp215f-stm32mp215dk-ashmx-mx.dts.  Stop.
make[1]: Leaving directory '/home/ashley/STM32MPU-Ecosystem-v6.2.0/Developer-Package/stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18/sources/ostl-linux/optee-os-stm32mp-4.0.0-stm32mp-r3-r0/optee-os-stm32mp-4.0.0-stm32mp-r3'
[OPTEE-OS BUILD ERROR] OPTEE_CONFIG: optee-programmer devicetree: stm32mp215f-stm32mp215dk-ashmx-mx
make: *** [/home/ashley/STM32MPU-Ecosystem-v6.2.0/Developer-Package/stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18/sources/ostl-linux/optee-os-stm32mp-4.0.0-stm32mp-r3-r0/optee-os-stm32mp-4.0.0-stm32mp-r3/../Makefile.sdk.stm32mp2:174: tee-optee-programmer-stm32mp21-stm32mp215f-stm32mp215dk-ashmx-mx] Error 1
FAILED > BUILD ISSUE on optee-os-stm32mp

Edit:

It would appear the problem is related to EXTDT_DIR_OPTEE_SERIAL not being set in Makefile.sdk.stm32mp2.  Setting this to default to EXTDT_DIR_OPTEE_SERIAL ?= $(EXTDT_DIR_OPTEE) resolves the issue.  Unfortunately it results in other errors further down the track, so may not be the root cause of the problem.  In the error messages below, the dts file name is correct, but the path to it is incorrect (it is the default path rather than external path).

Device Tree Source (arch/arm/dts/stm32mp215f-stm32mp215dk-ashmx-mx.dtb) is not correctly specified.
Please define 'CONFIG_DEFAULT_DEVICE_TREE'
or build with 'DEVICE_TREE=<device_tree>' argument

 

0 REPLIES 0