STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Boot to v5.4-stm32mp-r1

Hello,has anyone successful booted linux  v5.4-stm32mp-r1 on the stm32mp157c-dk2 board?If so can you please provide me a working config?I am trying to switch from the 4.19 kernel to v5.4-stm32mp-r1 but the boards freezes after trying to load the kern...

Artem by Associate III
  • 3327 Views
  • 5 replies
  • 0 kudos

Hello, I have a question regarding ST marketing on the STM32MP1 devices. According to the page, it states "STM32MP1 users can now choose from several IDEs from leading vendors and enjoy free license"

Which IDEs can be used for free in order to download/debug my application in an asynchronous fashion as two cores are running the the same time. I have taken a look on some suppliers (Tools & Software), but it looks like that you need to pay a some m...

PBart.3 by Associate II
  • 5987 Views
  • 10 replies
  • 1 kudos

Power startup with discrete power supply

Dear All,According to AN5256 "discrete power supply hardware integration" the power source for VDD is turned off in case of crash to "reset" the hardware using the PWR_ONRST signal. At startup. At cold startup and immediately after a crash the power ...

PGE by Associate III
  • 1160 Views
  • 2 replies
  • 0 kudos

dynamic memory size

In the stm32mp157C-DK2 board, there is a DDR3 memory with size 4GB x 1.I wanted to know why the size defined in the system is 512mb as the next figure show :

0693W000003PP7YQAW.png 0693W000003PP7iQAG.png
med by Associate II
  • 1818 Views
  • 4 replies
  • 0 kudos

Resolved! Error in recipe st-image-resize-initrd while building openstlinux-5.4-dunfell-mp1-20-06-24

Hello,​I always get following error while building openstlinux-5.4-dunfell-mp1-20-06-24:ERROR: st-image-resize-initrd-1.0-r0 do_rootfs: The postinstall intercept hook 'update_desktop_database' failed, details in /mnt/data/dist-pack/openstlinux-5.4-du...

DmnSd by Associate III
  • 4761 Views
  • 8 replies
  • 0 kudos

Resolved! How to use touchGFX on STM32MP1 ?

Hi @martin KJELDSEN​ , I have some questions related to porting touchGFX on STM32MP1 which are as below : 1) Is it possible to run touchGFX on M4 core available on STM32MP1 ? 2) As I understood earlier touchGFX was supported on ARM processors, If I h...

Shree by Associate II
  • 3617 Views
  • 5 replies
  • 0 kudos