STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Failed to download system image

Our self-made board contains emmc and lpddr3 (1GB, 32bit). The error message when downloading the image is as the attachment. Use Uart to monitor during the download process to get the following information:NOTICE: CPU: STM32MP157AAC Rev.Z NOTICE: Mo...

YWu.2 by Associate II
  • 4521 Views
  • 8 replies
  • 0 kudos

Using RAUC with openstlinux

We are using rauc to perform remote updates on your target devices.However, to create the rauc bundle, rauc uses a different image format than the ST image created.The default imagesource in rauc is:imgsource = "%s-%s.%s" % (d.getVar('RAUC_SLOT_%s' %...

meiss.M by Associate III
  • 4535 Views
  • 7 replies
  • 0 kudos

Resolved! STPMIC1 on I2C2 breaks ATF? Bug?

I'm currently working with the Seed STM32MP1 SoM which has STPMIC1 attached to I2C2. I've been working on setting up a device tree for it, but I've been hitting some bugs. When booting the mainline ATF with my device tree (modified DK2 board, just wi...

JGuy1 by Associate II
  • 2016 Views
  • 1 replies
  • 0 kudos