STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to get STM32Cube_FW_MP1_V1.2.0RC2?

want to exchange large data buffers with the coprocessor.I have done following wiki page.​https://wiki.st.com/stm32mpu-ecosystem-v1/wiki/How_to_exchange_large_data_buffers_with_the_coprocessor_-_example#Source_code​I want to analyze Cortex-M4 source ...

HMasu.1 by Senior
  • 1293 Views
  • 2 replies
  • 0 kudos

Resolved! Is there any sample source code that implements the transfer from Cortex-A to Cortex-M?

I want to implement the program that exchange large data with each other on Cortex-A7 and Cortex-M4 by using DDR.​Thanks to following wiki page, I have understand the mechanism that exchange large data from Cortex-M4 to Cortex-A7 by using DDR.​https...

HMasu.1 by Senior
  • 3442 Views
  • 6 replies
  • 0 kudos

Resolved! Trouble creating v2.0.0 bootable SD card with create_sdcard_from_flashlayout.sh. Is there a pre-built sdcard.img file available?

Following the instructions found in en.FLASH-stm32mp1-openstlinux-5-4-dunfell-mp1-20-06-24.tar.xz and using create_sdcard_from_flashlayout.sh to write the data to an SD card did not work for me. When I inserted the card on the stm32mp157c-dk2 dev bo...

BMaha.1 by Associate II
  • 3720 Views
  • 4 replies
  • 0 kudos

Resolved! Starting M4 from BootRom

Is there a way to directly start M4 and run M4 firmware from BootRom.I am aware of the Engineering mode, however it requires the help of a debugger to copy the M4 firmware into the memory and run it. I like to do the same but in stand alone mode.I am...