STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP1: OpenOCD cannot halt all cores

I am currently working on a design based around the STM32MP157C (mounted in the Seeed SoM - STM32MP157C).I am trying to connect to the M4 Core on the target but I cannot halt it. When I attempt to do it, the debugger can halt the A7 CPU0 but fails at...

bfh_dls by Associate II
  • 4482 Views
  • 3 replies
  • 0 kudos

Needs support the Windows 10 IoT

Hi all,Windows 10 IoT Core already supports run on the single ARM Cortex-A7 MPU! Is there a BSP of the STM32 MPU that can be used for the Windows 10 IoT?Refer here:https://docs.microsoft.com/en-us/windows/iot-core/learn-about-hardware/socsandcustombo...

I made a board with the official STM32MP157 and got the following error when measuring the CPU frequency

The kernel I used was 4.19 and the CPU on STM32MP157AAA3 was able to read the CPU at 650M frequency.I failed to read when I only replaced THE CPU with STM32MP157DAA1.STM32MP157AAA3 To read the CPU frequency results are as follows:STM32MP157DAA1 Reads...

0693W000004H6DxQAK.png 0693W000004H6OnQAK.png
User.44 by Associate II
  • 1096 Views
  • 1 replies
  • 0 kudos