STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Good afternoon, Olivier. Thanks for the help. But I saw a problem with MPU Serial (COM3). I ran ipconfig in Linux and found the real address of usb0 192.168.7.2.

Good afternoon, Olivier. Thanks for the help. But I saw a problem with MPU Serial (COM3). I ran ipconfig in Linux and found the real address of usb0 192.168.7.2 after that, the console worked.But the board does not allow debugging. I must have done s...

Vlaty.1 by Senior
  • 1096 Views
  • 0 replies
  • 0 kudos

Resolved! M4 Core ITM trace

Hi,Looking at the reference manual, en.DM00327659.pdf, page 3929 it seems the simple way of debugging previous M4 processors using printf() redirect to the ITM and then using the SWO pin/STLINK interface could be used on the MP1 M4 core as well.But t...

K.Ata15 by Associate III
  • 3652 Views
  • 5 replies
  • 1 kudos