STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! U-boot Animated Splash screen

Hi all,How can i add support for animated splash screen on stm32mp1 ?I have understanding of the psplash recipe used for custom bootscreen which works completely fine. I would like to have animation while system is booting up.Any inputs are highly ap...

NPal.2 by Senior
  • 5354 Views
  • 2 replies
  • 0 kudos

Resolved! USB Composite in STM32MP157c

I am struggling to achieve a USB gadget with Mass Storage + rndis.When i start each service alone everything works but when i am trying to start both of them i receive the following error:dwc2_hsotg_ep_enable: No suitable fifo foundAny suggestion how...

AKokk by Associate II
  • 4834 Views
  • 5 replies
  • 1 kudos

Resolved! On the STM32MP157C-DK2, can I use/interface the available muRata 1Dx with M4 only (& not A7)?

On the STM32MP157C-DK2, can I use/interface the available muRata 1Dx with core-M4 only (& not core-A7)? I am not quite sure if the wifi module 1dx (U8 on the kit) is controlled by A7 or M4?Anyways, I want to interface it with M4. So, can it be possib...

ANalg.1 by Associate II
  • 3004 Views
  • 2 replies
  • 0 kudos