STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

modify a CAN sample point

I using a STM32MP-157F-EV1 eval board with linux Version 4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15.CAN receive 500kBit/s fails, if I modify the sample point via an console command it works well. All other Bitrates 125kBit / 250kBit 1MBit a...

MaHa by Associate II
  • 3529 Views
  • 5 replies
  • 1 kudos

Resolved! STM32MP1) Occasionally eMMC boot fail with "CMD13 failed after 5 retries"

​Hi all ~​I have STM32MP157C custom board. My custom board boot over eMMC. Occasionally, my board can not boot over eMMC with error message like below.Can I get some advice regarding this problem?Hardware of eMMC part is the same as EV1 board. ​Thank...

GPIO changes with Linux v5.15

I've upgraded from 5.10 to 5.15 and can't make GPIO work anymoreI've tried thisgpio_keys { compatible = "gpio-keys"; input-name = "gpio-keys"; status = "okay";   halt { label = "Halt"; linux,code = <KEY_POWER>; // Key event to match wit...

fpoussin by Associate III
  • 4605 Views
  • 4 replies
  • 0 kudos