STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP1 FDCAN issues

Hello,I have the stm32mp157c-dk2 board and have connected two CAN Bus transceivers to it.FDCAN1 is assigned to the A7 CPU and the FDCAN2 is assigned to the M4 CPU.Both transmitters are connected to the same CAN bus. There is also a 3rd device connect...

Artem by Associate III
  • 14456 Views
  • 22 replies
  • 0 kudos

Start M4 firmware automatically

Hi!I am using STM32MP157C-DK2 and i want to start the coprocessor from bootloader (I have readed the wiki page). First, I have done it manually and everithing works fine:I have changed kernel m4_rproc:&m4_rproc{ /*Restriction: "memory-region" proper...

JIrao.1 by Associate
  • 2675 Views
  • 3 replies
  • 0 kudos

Resolved! ETZPC and kernel FIT image

Hi all!!Follow the wiki page, I added support to kernel FIT image in my Yocto distro for the board stm32mp157c-dk2 based on openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23.Just I added the option: MACHINE_FEATURES += "fit" and I selected BOOTSCHEME_LA...

AVazquez by Associate III
  • 4999 Views
  • 2 replies
  • 0 kudos

Resolved! Cortex-M4 is not running In uboot With Rproc commands for stm32mp157a processor.

Hi,We are using stm32mp157a-dk1 board. In this when we boot Cortex-M4 code with rproc commands in uboot, cortex-M4 is running.We are using stm32mp157aaa3 processor in my custom board. When we are trying to boot Cortex-M4 in Uboot with rproc commands....

Resolved! STM32MP1-CortexA7 SDMMC1 TxUnderrun Error

Hi, community.​I am trying the SD UHS-I mode on your evaluation board(STM32MP157F-EV1), but it does not work.Q1. Does HAL support UHS-I?​Q2. Is it necessary to enable SDMMC_CLKCR_SELCLKRX_1? (when using STM32MP157F-EV1 board)Q3. What is the reason wh...

TSens.1 by Associate II
  • 1556 Views
  • 1 replies
  • 0 kudos