2023-01-25 1:40 AM
Hi all!!
Follow the wiki page, I added support to kernel FIT image in my Yocto distro for the board stm32mp157c-dk2 based on openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23.
Just I added the option: MACHINE_FEATURES += "fit" and I selected BOOTSCHEME_LABELS += "trusted" in stm32mp15-disco.conf and finally I generated the new image.
The problem is thar after start kernel I see a ETZPC trace that does not appear in the typical configuration.
FIT image traces:
## Loading kernel from FIT Image at c2000000 ...
Using 'conf-stm32mp157c-dk2.dtb' configuration
Trying 'kernel-1' kernel subimage
Description: Linux kernel
Created: 2022-09-08 10:32:54 UTC
Type: Kernel Image
Compression: uncompressed
Data Start: 0xc2000120
Data Size: 7903152 Bytes = 7.5 MiB
Architecture: ARM
OS: Linux
Load Address: 0xc0800000
Entry Point: 0xc0800000
...
Verifying Hash Integrity ... sha256+ OK
## Flattened Device Tree blob at dbb017b0
Booting using the fdt blob at 0xdbb017b0
Loading Kernel Image
Loading Ramdisk to cfc21000, end cfffffe1 ... OK
Loading Device Tree to cfc00000, end cfc206c7 ... OK
ETZPC: 0x5a003000 node disabled, decprot 10=1NO FIT traces:
Retrieving file: /uImage
7903216 bytes read in 645 ms (11.7 MiB/s)
Retrieving file: /st-image-resize-initrd
4059103 bytes read in 404 ms (9.6 MiB/s)
append: root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200
Retrieving file: /stm32mp157c-dk2.dtb
118549 bytes read in 156 ms (741.2 KiB/s)
## Booting kernel from Legacy Image at c2000000 ...
Image Name: Linux-5.15.67
Created: 2022-09-08 10:32:54 UTC
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 7903152 Bytes = 7.5 MiB
Load Address: c2000040
Entry Point: c2000040
Verifying Checksum ... OK
## Flattened Device Tree blob at c4000000
Booting using the fdt blob at 0xc4000000
XIP Kernel Image
Loading Ramdisk to cfc21000, end cfffffdf ... OK
Loading Device Tree to cfc01000, end cfc20f14 ... OK
Starting kernel ...Besides, in the kernel logs, I see some changes for example, it changes the I2C bus where the devices are located.
FIT Kernel trace:
[ 2.144266] i2c 4-0039: Fixing up cyclic dependency with 4000b000.audio-controller
[ 2.150680] i2c 4-0039: Fixing up cyclic dependency with 5a001000.display-controllerNormail Kernel trace:
[ 2.118101] i2c 0-0039: Fixing up cyclic dependency with 4000b000.audio-controller
[ 2.124495] i2c 0-0039: Fixing up cyclic dependency with 5a001000.display-controllerAre any additional steps necessary for use kernel FIT with the distro openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23?
Is it possible to disable the ETZPC node? In previous versions of tf-a it was disabled by default but in this commit, it says it is always enabled.
Thanks!
A.
Solved! Go to Solution.
2023-01-30 2:01 AM
It's a bug with FIT image and exlinux.conf
In this commit, the oficial repo u-boot revert the commit "cmd: pxe_utils: Check fdtcontroladdr in label_boot"
https://github.com/u-boot/u-boot/commit/ed6251187afabf811a5fd49a44ebd61c53c7b378
For stm32 u-boot it's necesary revert this commit.
Regards.
A.
2023-01-26 12:42 PM
2023-01-30 2:01 AM
It's a bug with FIT image and exlinux.conf
In this commit, the oficial repo u-boot revert the commit "cmd: pxe_utils: Check fdtcontroladdr in label_boot"
https://github.com/u-boot/u-boot/commit/ed6251187afabf811a5fd49a44ebd61c53c7b378
For stm32 u-boot it's necesary revert this commit.
Regards.
A.