Hi,How can I install a USB serial adaptateur https://ftdichip.com/products/chipi-x10/When the usb adaptateur is connected there is not ttyS0 or ttyUSB0 !thank you.
Hi,
Each time I reboot my Discovery kit with STM32MP135F borad I lost the network (IP V4 address).
How can I set the IP address, Does exits somewhere a /etc/network/interface file ?
Thank you,
Olivier.
Thanks Jean-Marc,It's ok now I've been able to install pyserial.I know I need to update the OpenSTLinux image but for that I need a VM with linux on my laptop and I need authorization from my company to install it. I'll do it as soon as possible.Than...
Hello Jean-Marc, Andrew,I thing I am connected with internet (I not sure).If I test : (see bellow the error message) apt-get update root@stm32mp1:/etc/wpa_supplicant# apt-get updateThe software package is provided AS IS, and by downloading it, you ag...
I want to use static IP address like 192.168.0.10.so I send :ifconfig eth0 192.16.0.10 netmask 255.255.255.0then it worksbut if i reboot the board I lost the network.I would like to know wich file I need to setup.Thank you