STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Why is GMII designed for STM32MP dev kit?

Hi!I notice something!In the devkit of STM32MP15xxxx, I found that ETH_TX_EN is used for GMII, but when I check the CubeMX, I found that RGMII is used instead. This is the settings for RGMII. In the devkit schematics, it is ETH1_TX_EN, not ETH1_TX_CT...

Skärmbild 2024-05-11 131350.png Skärmbild 2024-05-11 130641.png Skärmbild 2024-05-11 130902.png Skärmbild 2024-05-11 131231.png
DMårt by Lead
  • 1897 Views
  • 1 replies
  • 1 kudos

debuging problem

I'm attempting to debug an STM32MP157 using STM Cube IDE on Windows, but I've encountered an issue with a parameter, and I'm unsure of its origin. Could you provide assistance with this matter?   

fadi_chwayet_0-1715336193098.png fadi_chwayet_1-1715336239461.png

STM32MP1 openstlinux hardware access

Hi there, we are developing a custom STM32MP135 board to run openstlinux on it. It will be our first experience with embedded linux (linux) systems, so we have some tasks that we don't know if it can be done. These tasks are the following:Can we acce...