cancel
Showing results for 
Search instead for 
Did you mean: 

USB HID doesn't work without hub

Dat Tran
Senior II

Hi, when I inserted keyboard/mouse to USB host port, nothing happened (log console) and this even cause usb host stop working then.

But when I inserted keyboard/mouse to a hub and connect this hub to usb host port, everything working fine.

The problem is only happened with hid (keyboard/mouse). When I used USB thumb drive, it works just fine, no need the hub.

The chip I used is STM32MP153 and this is custom build

Does anyone know why or any hint?

Thanks.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Dat Tran
Senior II

I got it working. Need to enable ochi driver in device tree.

View solution in original post

2 REPLIES 2
Dat Tran
Senior II

I got it working. Need to enable ochi driver in device tree.

I have a similar error but in device mode, if I connect my board to the PC without HUB there are big chances that it wont work, but when I use a hub it always is recognise be the PC. 

 

Which drive did you precisely enable and where? Can you load some screen captures?

 

Thanks in advance.