STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Error: unable to get the associate alternate setting of partition ID: 0xf1 With Kirkstone distro

Hi, I miograting to Kirkstone distro on mu custom board and i have this issue with programming the board: and i cannot understrand what this error mean, can somebody explain it where i am wrong? because on Dunfell it worked perfect. the Yocto compili...

SMich.1 by Senior
  • 3254 Views
  • 2 replies
  • 0 kudos

STM32MP157 uboot issue

When I download UBOOT using USB, the console appears the following log and repeats. Is this normal? I was wondering if when I modified uboot, it didn't fully fit my board?NOTICE: CPU: STM32MP157AAA Rev.BNOTICE: Model: STMicroelectronics STM32MP157A e...

lijingyu by Associate
  • 1715 Views
  • 1 replies
  • 0 kudos

How to connect the printer

HiI got cups and hplip by adding IMAGE_INSTALL_append = "python3-distro cups ghostscript cups-filters hplip"  in local.conf.but when I run hp-check, there are some errors about missing required dependencies : root@STM32MP1:~# hp-check /usr/bin/hp-che...

macrobert by Associate II
  • 3825 Views
  • 4 replies
  • 0 kudos

Resolved! STM32MP135 - Azure RTOS - TraceX

Hello, is there a possibility to apply TraceX to a ThreadX project using MP135? I could follow some tutorials and include the necessary TraceX functions, but I can't generate a .trx file. The option is simply not available in the CubeIDE. Would you h...