hdma_tim1_ch1.XferCpltCallback = TransferCompleteCallback; IS NOT TRIGGERIING
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-11 10:11 PM - edited ‎2024-08-18 4:32 AM
I am transfering data array from an array to PWM register of TIM1.
int16_t sin_table[20]= { 0, 39, 77, 113, 147, 177, 202, 223, 238,247, 250, 247, 238, 223, 202, 177, 147, 113, 77, 39};
HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_1, (uint32_t *)sin_table, 20);
And i am trying to blink in complete transfer callback fuction as follows .
I am getting PWM signal as expected . but trigger the TransferCompleteCallback).
by using break poiint the DMA Inerupt Handler triggers but not trigger the callback i said .
whats the wrong am with please help me .
i am attaching the full code here
aNY BODY HELP ME
Solved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-20 6:56 AM
Ok seems you dont show STM32 xx ?? Ok when you build with defined USE_HAL_TIM_REGISTER_CALLBACKS == 1
#if (USE_HAL_TIM_REGISTER_CALLBACKS == 1)
htim->OC_DelayElapsedCallback(htim);
htim->PWM_PulseFinishedCallback(htim);
#else
HAL_TIM_OC_DelayElapsedCallback(htim);
HAL_TIM_PWM_PulseFinishedCallback(htim);
#endif /* USE_HAL_TIM_REGISTER_CALLBACKS */
}
htim->Channel = HAL_TIM_ACTIVE_CHANNEL_CLEARED;
hope you now see how and when register callbacks.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-18 4:33 AM - edited ‎2024-08-19 9:48 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-18 4:54 AM
Seems you missunderstan HAL callbacks ... read examples in folder repository firmware for your MCU...
You mark all MCUs, this isnt very helpfull. For example F4 from stm32f4xx_hal_tim.c func HAL_TIM_PWM_Start_DMA
switch (Channel)
{
case TIM_CHANNEL_1:
{
/* Set the DMA compare callbacks */
htim->hdma[TIM_DMA_ID_CC1]->XferCpltCallback = TIM_DMADelayPulseCplt;
htim->hdma[TIM_DMA_ID_CC1]->XferHalfCpltCallback = TIM_DMADelayPulseHalfCplt;
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-19 2:02 AM - edited ‎2024-08-19 2:03 AM
Hi Thanks , I didnt find any examples related DMA transfer complete function trigger based projects .
Hi may i need to register the following function to trigger the calla back function
HAL_DMA_RegisterCallback(&hdma, HAL_DMA_XFER_CPLT_CB_ID, My_DMA_TransferCompleteCallback);
Or any other way to do this , is there tutorials or mannual for it ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-19 7:32 AM
Simply HAL prepare weak for you and yu cant choice any func, but need overide.
/**
* @brief PWM Pulse finished callback in non-blocking mode
* @PAram htim TIM handle
* @retval None
*/
__weak void HAL_TIM_PWM_PulseFinishedCallback(TIM_HandleTypeDef *htim)
{
/* Prevent unused argument(s) compilation warning */
UNUSED(htim);
/* NOTE : This function should not be modified, when the callback is needed,
the HAL_TIM_PWM_PulseFinishedCallback could be implemented in the user file
*/
}
then rename in your code void TransferCompleteCallback to HAL_TIM_PWM_PulseFinishedCallback(TIM_HandleTypeDef *htim)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-19 8:34 AM - edited ‎2024-08-19 9:36 PM
Hi
HAL_TIM_PWM_PulseFinishedCallback(TIM_HandleTypeDef *htim) is used for one complete cycle isnt it ?
or one ARR value
I registred the callback as follows
HAL_DMA_RegisterCallback(&hdma_tim1_ch1,HAL_DMA_XFER_CPLT_CB_ID,GKS);
void GKS(DMA_HandleTypeDef*hdma)
{
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_SET);
}
hdma->XferCpltCallback = pCallback; // this code executed while debugging but the above GKS function is not triggering
why so ,is there any oher need to enable ?
@Sarra.S
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-20 1:57 AM
Hello @thannara123,
>>i am attaching the full code here
I cannot see the full code, could you share it?
The registration of the callback using HAL_DMA_RegisterCallback needs to be done before starting the DMA transfer using HAL_DMA_Start.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-20 6:56 AM
Ok seems you dont show STM32 xx ?? Ok when you build with defined USE_HAL_TIM_REGISTER_CALLBACKS == 1
#if (USE_HAL_TIM_REGISTER_CALLBACKS == 1)
htim->OC_DelayElapsedCallback(htim);
htim->PWM_PulseFinishedCallback(htim);
#else
HAL_TIM_OC_DelayElapsedCallback(htim);
HAL_TIM_PWM_PulseFinishedCallback(htim);
#endif /* USE_HAL_TIM_REGISTER_CALLBACKS */
}
htim->Channel = HAL_TIM_ACTIVE_CHANNEL_CLEARED;
hope you now see how and when register callbacks.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-20 8:14 AM
@thannara123,as MM says, your code is not doing what you think it's doing.
1. By default, when Cube generates code it leaves USE_HAL_TIM_REGISTER_CALLBACKS undefined.
2. When this is undefined the HAL registers and calls its own, default, callback handlers for each event.
3. This handlers are generated as part of the code but are annotated as "weak" in the code.
4. Weak symbols are compiler/linker feature that allows you to override that symbol (function) with your own implementaiton. All you need to do is to implement the same function (name, and signature) in your own code (without the "weak" annotation) and then it will be used instead of the weak function/symb
Alternatively, you can define USE_HAL_TIM_REGISTER_CALLBACKS, or check the box in CubeMX GUI that does this for you. Once that is defined, you can use RegisterCallback to register your own callback, and the HAL generated code (using an ifdef USE_HAL_TIM_REGISTER_CALLBACKS) will invoke it.
- Please post an update with details once you've solved your issue. Your experience may help others.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-20 9:54 PM - edited ‎2024-08-20 10:05 PM
Thanks for the knowlegde sharing .
Actually I require the callback function is whenever complete the full arrray throgh DMA , DMA will trigger the TCIF flag .SO then i require a user defind callback .so I registred a call back function as follows
HAL_DMA_RegisterCallback(DMA_HandleTypeDef *hdma, HAL_DMA_CallbackIDTypeDef CallbackID, void (* pCallback)(DMA_HandleTypeDef *_hdma))
{
HAL_StatusTypeDef status = HAL_OK;
/* Process locked */
__HAL_LOCK(hdma);
if(HAL_DMA_STATE_READY == hdma->State)
{
switch (CallbackID)
{
case HAL_DMA_XFER_CPLT_CB_ID:
hdma->XferCpltCallback = pCallback; // it will trigger or give 1 , upon the full transfer
break; //
HAL_DMA_RegisterCallback(&hdma_tim1_ch1,aCallbackIDTypeDef,Usrdefnd_Complete_callback);
void Usrdefnd_Complete_callback(DMA_HandleTypeDef*hdma)
{
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_SET);
}
I tried like wise but not worked .
Also I tried the follwsing type of callback
hdma.XferCpltCallback = MyDMA_TransferCompleteCallback; //But not worked as expected
I doubt as follows
HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_1, (uint32_t *)sin_table, 20);//low
HAL_TIMEx_PWMN_Start_IT(&htim1, TIM_CHANNEL_1);
Here I am not used IT in the HAL_TIM_PWM_Start_DMA funtion , is it make any problem ?
anyway the cube ide enabled the DMA2 stream 1 and 2 as shown below .