cancel
Showing results for 
Search instead for 
Did you mean: 

How do I measure motors with the EVSPIN32G4 board?

SUNGHWANCHO
Associate II

I found the motor value using the Motor Profiler 5.4.8 program (P-NUCLEO-IHM002).
(Figure1)

The Motor Pilot_6.3.0 program does not connect using UART.(Discover Board / Launch Profiler)
(Figure3)

Even if I change the UART Speed, the "Port Open and try to configure the board" error only appears.
(Figure4)

I bought EVSPIN32G4 to run the motor at 60v voltage level.

However, I understand that motor measurement is currently not possible with the Motor Profiler 5.4.8 program.

In that case, you need to measure it in the Motor Pilot_6.3.0 program.

I can't check anything because the connection isn't working.

MC_Workbench cannot create a project because there is no motor with similar specifications.

Since I cannot receive the motor value from the motor manufacturer, I have to proceed through measurement. Please tell me how I can do this.

3 REPLIES 3
GMA
ST Employee

Hello @SUNGHWANCHO,

Please have a look to How_To_manually_configure_the_motor_parameters link.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA

After purchasing EVSPIN32G4, I only updated ST-LINK after connecting Micro USB.

stlink.JPG

It is connected to the motor as shown below.

5.jpg

The board cannot be connected in ST Motor Pilot.

SUNGHWANCHO_0-1720572668367.png

How do I connect?

kelvin.wang
Associate II

MCSDK 6.3 Profile need user to add FW manually by create new project ,you may refer to MCSDK document in "about" ICON and search "Motor Profiler Application Note"