2024-07-09 1:48 AM
Hello everyone,
I’m currently working on a motor control project using a custom board with STSPIN32G4 and STDRIVE101, which is similar to the EVSPIN32G4. I’m trying to control two motors, and I have implemented a single shunt resistor for current sensing.
Some suggest using Motor Profiler to ensure the motor parameters are correct, but clearly, I’m unable to use Motor Profiler because it does not support a single shunt resistor configuration.
For the speed tracking issue, maybe I can try using Motor Pilot? However, when attempting to use Motor Pilot and loading MC_FOC_SDK.qml, I encounter the error “ASPEP PACKET UNKNOWN”.
Any guidance or recommendations would be greatly appreciated!
Thank you!
Yan-Liang Chen
2024-07-10 2:05 AM
Additional question: Since I'm using a custom board, am I able to use Motor Pilot?
2024-07-12 5:59 AM
Hi, Have you find a solution for your problem? I am dealing with the same issue.