cancel
Showing results for 
Search instead for 
Did you mean: 

B-G431B-ESC1 with FOC

sambit_das
Associate II

I am trying to run an A2212 13T motor with B-G431B-ESC1 motor with FOC algorithm.But the motor gets stopped after attaining a low speed.Solve the problem.

2 REPLIES 2
MotorRunner
Associate III

if you're running the motor in the sensorless mode, it is no Surprise it stops when running at a very low speed.

probably, the current consumption is vey low in such a way that the foc firmware cannot measure, then your motor stops

regards

I want to rotate that motor to the max speed with Sensorless FOC with observer pll.I am changing the speed through st motor pilot gui up to the max speed.But still the motor is stopping at low speed.How to resolve the issue?