ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ST25R95 maximum voltage of VRX1/2?

Hello,Just a clarification question. When going through the application note (AN5248) for ST25R95. It mentiosn at one point there is a maximum allowed voltage on RX1 and RX2 which should be below 7V.Where in the datasheet is this specified? Thank you...

tyassin_0-1712561853210.png
tyassin by Associate III
  • 1594 Views
  • 5 replies
  • 0 kudos

Resolved! NFC card reader for ST25DV16KC tag

Hi,I'm working with the ST25DV16KC-IE6T3 tag (ISO15693 type 5) and I want to both read and write data to it.I'm looking for a compatible NFC card reader that can connect to the computer via USB port (either desktop PC or laptop.)The use case would be...

KKulk.1 by Associate
  • 1197 Views
  • 2 replies
  • 0 kudos

Resolved! ST25DV password protection

I activated the area1 password protection with password 1. I saw that the default password is "0". Is there a way to change the password 1 over the I2C or is it only possible to change it from NFC side?I saw that all RF_PWD witch can be configurated ...

SimoE by Associate II
  • 1263 Views
  • 1 replies
  • 0 kudos

Resolved! ST25DV GPO Interrupt

I'm trying the ST25DV, ( open drain connection with pullup resistor of 20k ) but I can't get the interrupt to work through the GPO pinThe product code read is 0x51I wrote the register with GPO_EN = 1 and RF_ACTIVITY_EN = 1, RF_WRITE_EN =1, FIELD_CHAN...

Diego72x by Associate II
  • 1778 Views
  • 4 replies
  • 0 kudos

Unable to Download Software

I'm trying to download a software, but a message appears "This software is not available for download". But when I sign out and try to download as a guest I receive a link in my inbox and the download starts. how can I solve this issue to download di...

Resolved! NFC Tap Source Code

Hello,i downloaded the source code of the iOS App (STSW-ST25IOS001), but i get tons of error, it's not compilable.Has anyone tried? I wanted to use it as reference for developing.I already made an app with Android and it's working, with far less trou...

giorgio86 by Associate II
  • 1738 Views
  • 6 replies
  • 0 kudos

Resolved! ST25 SDK for .NET

Is there a .NET SDK for ST25 NFC tags that will let me read and write ISO 15693 Type 5 tags in C#? I have the ST25R3911B-DISCO reader/writer board.The closest I've found so far is a COMMS dll which appears to be taken from the demo app and will not l...

TimLong by Associate III
  • 2065 Views
  • 5 replies
  • 1 kudos