2023-12-28 8:39 PM
float K_Temperature ; //K型热电偶 温度值
char temperaturebuffer[30] = { 0xD1, 0x01, 0x1B, 0x54, 0x02, 0x65, 0x6E };
uint16_t TarAddr= 0x0000;
/* Write NDEF to EEPROM */
K_Temperature=MAX6675_ReadTemperature(); //读取热电偶温度值
sprintf(&temperaturebuffer[7], "Temperature: %.2f C", K_Temperature);
NFC07A1_NFCTAG_WriteData(NFC07A1_NFCTAG_INSTANCE, (uint8_t *)temperaturebuffer, TarAddr, strlen(temperaturebuffer) + 1);
uint8_t ReadData[30];
NFC07A1_NFCTAG_ReadData(NFC07A1_NFCTAG_INSTANCE, ReadData, TarAddr, sizeof(ReadData));
// 延时一段时间
HAL_Delay(300);
NFC07A1_LED_On( GREEN_LED );I converted the temperature data into a string and wrote it to the address, but NFC couldn't get the temperature information. I don't know if it's a write function usage error or a write address error, but here's what NFC gets.
Solved! Go to Solution.
2024-01-02 12:56 AM
Hi,
if your application is supposed to write the temperature data as a TEXT NDEF record, the tag has to be properly NDEF formatted (i.e. with a Capability Container starting at block 0 followed by an NDEF TLV). See
2023-12-29 7:18 AM
Hi,
see the first reply of https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/x-cube-nfc7-no-ndef-seen-by-the-phone/td-p/144185: NFC07A1_NFCTAG_WriteData writes raw data into the tag and therefore this is not NDEF formatted.
Rgds
BT
2023-12-29 7:24 AM
Hi @Brian TIDAL
But what I am writing is sensor data, which is dynamic data. Can I follow the above reference? Is there a specific method for writing NFC into sensors?
2023-12-29 9:21 AM
HI,
I've just seen that temperaturebuffer contains an NDEF TEXT record header (D1 01 etc.). So I assume you write the temperature value inside a TEXT record. But as TarAddr equals 0, this NDEF is written by NFC07A1_NFCTAG_WriteData at block 0 whereas block 0 should contain the NFC Forum Capability Container. Therefore the tag is no longer properly formatted.
I would suggest to reuse X-CUBE-NFC7\1.0.0\Projects\NUCLEO-L476RG\Applications\NDEF_URI in your application and to modify it to use a TEXT record instead of an URI record.
If you still prefer to use NFC07A1_NFCTAG_WriteData, make sure to have a Capability container in block 0 and the NDEF Type and Length fields before the NDEF TEXT record.
Rgds
BT
2023-12-29 6:52 PM
Hi @Brian TIDAL
I tried using NfcTag_ WriteNDEF can display temperature data correctly in text form, but I am currently debugging STEVAL-SMARTAG1, and the code does not include NDEF related function definitions, only NFCTAG_ WriteData and NFCTAG_ ReadData, do you have any suggestions for me to try to read temperature data?
2024-01-02 12:56 AM
Hi,
if your application is supposed to write the temperature data as a TEXT NDEF record, the tag has to be properly NDEF formatted (i.e. with a Capability Container starting at block 0 followed by an NDEF TLV). See
2024-01-03 12:19 AM
Hi @Brian TIDAL
Thank you for your answer. According to the instructions of AN4911, I can only know the theoretical knowledge of NDEF, but I currently need to read the dynamic temperature data without code instructions, how should I deal with K_Temperature in the software design?
K_Temperature=MAX6675_ReadTemperature(); // Read the thermocouple temperature value.
2024-01-03 12:47 AM
Hi,
I am sorry but I do not understand your last post. I am afraid I cannot help more.
Rgds
BT
2024-01-03 1:23 AM
Hi @Brian TIDAL
I know the Capability Container starting at block 0 followed by an NDEF TLV, I change the write address to 0XD1, which is block 01:03 11 D1 01: NDEF TLV (T=03h, L=11h,), can the following corrected code write temperature data correctly?
float K_Temperature ;
char temperaturebuffer[30] = { 0xD1, 0x01, 0x1B, 0x54, 0x02, 0x65, 0x6E };
uint16_t TarAddr= 0xD1;
void MX_NFC7_NDEF_URI_Init(void)
{
/******************************************************************************/
/* Configuration of X-NUCLEO-NFC02A1 */
/******************************************************************************/
/* Init of the Leds on X-NUCLEO-NFC07A1 board */
NFC07A1_LED_Init(GREEN_LED );
NFC07A1_LED_Init(BLUE_LED );
NFC07A1_LED_Init(YELLOW_LED );
NFC07A1_LED_On( GREEN_LED );
HAL_Delay( 300 );
NFC07A1_LED_On( BLUE_LED );
HAL_Delay( 300 );
NFC07A1_LED_On( YELLOW_LED );
HAL_Delay( 300 );
/* Init ST25DVXXKC driver */
while( NFC07A1_NFCTAG_Init(NFC07A1_NFCTAG_INSTANCE) != NFCTAG_OK );
/* Reset Mailbox enable to allow write to EEPROM */
NFC07A1_NFCTAG_ResetMBEN_Dyn(NFC07A1_NFCTAG_INSTANCE);
NfcTag_SelectProtocol(NFCTAG_TYPE5);
/* Check if no NDEF detected, init mem in Tag Type 5 */
if( NfcType5_NDEFDetection( ) != NDEF_OK )
{
CCFileStruct.MagicNumber = NFCT5_MAGICNUMBER_E1_CCFILE;
CCFileStruct.Version = NFCT5_VERSION_V1_0;
CCFileStruct.MemorySize = ( ST25DVXXKC_MAX_SIZE / 8 ) & 0xFF;
CCFileStruct.TT5Tag = 0x05;
/* Init of the Type Tag 5 component (M24LR) */
while( NfcType5_TT5Init( ) != NFCTAG_OK );
}
/* Init done */
NFC07A1_LED_Off( GREEN_LED );
HAL_Delay( 300 );
NFC07A1_LED_Off( BLUE_LED );
HAL_Delay( 300 );
NFC07A1_LED_Off( YELLOW_LED );
HAL_Delay( 300 );
}
/**
* @brief Process of the NDEF_URI application
* @retval None
*/
void MX_NFC7_NDEF_URI_Process(void)
{
/* Write NDEF to EEPROM */
K_Temperature=MAX6675_ReadTemperature();
sprintf(&temperaturebuffer[7], "Temperature: %.2f C", K_Temperature);
NFC07A1_NFCTAG_WriteData(NFC07A1_NFCTAG_INSTANCE, (uint8_t *)temperaturebuffer, TarAddr, strlen(temperaturebuffer) + 1);
uint8_t ReadData[NFCTAG_64K_SIZE];
NFC07A1_NFCTAG_ReadData(NFC07A1_NFCTAG_INSTANCE, ReadData, TarAddr, strlen(temperaturebuffer) + 1);
HAL_Delay(300);
NFC07A1_LED_On( GREEN_LED );
}