User Activity

we are observing weird error during initilization...enclosed the log dump (board2_init_fail_log.txt and ll13_01_board2_success_logs.txt)on Raspberry pi with 2 NFC03A1 boards (SPI3.0 works well, SPI0.0 fails)2 independent binaries are being used with ...
 we are attempting to read wristband mifare classic tag using NFC03A1NFC03A1 is able to detect the tag UID.when we execute ndefPollerReadBytes().. directly, we get ret = 04 (ERR_TIMEOUT)need some sample code to read this tag...from your forum i under...
pls suggest a example for reader/writer/formatter for NFC03A1are there any writer example code for RPi similar to poller example ?https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/x-cube-nfc3-for-stm32cube/td-p/591339i didnot find the source...
wanted suggestions on SW integration to handle 2/3 NFC03A1 boards with RPi4HW SPI connections seems to be okon the SW side, how to handle multiple spi.Pls advise 
HW : Raspberry PI 4 with NFC03A1 board connected to SPISW : Linux_RFAL_st25r95_v2.0.4.tar.gzwe built and we are able to run on the Rpi board, poller exampleissue :ISO1444A tag not detectedSPI seems to be working, we observed IDN command responds with...
Kudos from