How to improve ST25R3916 2nd and 3rd Harmonic filtering?
With the ST25R3916, how can filtering of the 3rd harmonic (40.5 MHz) be improved? Following the procedure outlined in AN5276, a matching network was made. Performance of the device was verified, and emissions in the 13.56 MHz band are within FCC limits. However, the 3rd harmonic is above acceptable levels. Measurements with a near field probe on the tag show similar levels of the 3rd harmonic in the device I am using and the NUCLEO-NFC06A1 test board.
Changes that have attempted but did result in changes to the measured field on a near field probe:
Changing the cutoff frequency of the EMC filter (11 MHz, 13.8MHz, 15.5 MHz)
Changing the damping resistor
Changing the driver resistance
Changing regulator voltage
Are there other recommended approaches to reduce this harmonic?