ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ST25R3918: Unstable efd_o bit in Auxiliary Display Register after NFC-F Card Emulation response

Hello,I am using the ST25R3918 controlled by an MCU via RFAL, operating in NFC-F / FeliCa card emulation mode.I am monitoring the efd_o bit (bit 6) of the Auxiliary Display Register (Address: 31h) to detect when the board approaches an external reade...

Tyama.1 by Associate II
  • 115 Views
  • 4 replies
  • 1 kudos

Resolved! ST25R100 NFC Tag Read Problems

Hi everyone,I’m trying to interface an ST25R100 NFC reader with my MCU, and I’m having trouble reading ISO15693 tags. My initialization seems to work, but I never get any response from the tag. I’m hoping someone can spot what I might be missing.This...

Resolved! ST25R3911B SPI issues

Hello,I got back to my issues from this post.I was able to connect wires to SPI lines, and get the measurements to logic analyzer. These are the results:Logic2 screenshot Now i can see that the issue is the CS line, but i dont know why it is being ch...

Screenshot from 2026-01-27 12-45-23.png qwdwdwwq_0-1769517959549.png
qwdwdwwq by Associate II
  • 261 Views
  • 11 replies
  • 9 kudos

Resolved! where to get blank NFC card to write image developed by STM32L476RG and X-NUCLEO-NFC07A1 board

I'm developing a new secret card project using STM32L476RG and X-NUCLEO-NFC07A1 board, I plan to let the secret card to store private key and do signature related tasks. I'm not sure where can I get blank card which contains the same MCU with STM32L4...

dingchaojie_0-1769419631065.jpeg dingchaojie_1-1769419691377.png

Resolved! IBIS model ST25R200

Hi, I'm performing for a customer a signal integrity simulation involving ST25R200 (SPI interface). Is there any IBIS model available for this component (or ST25R100)? Thanks, RegardsRoberto