2025-06-09 8:44 AM
Hello everyone,
I am currently using a custom NFC board based on the X-Nucleo-NFC08A1 that has the ST25R3920B MCU. I am able to perform OOB pairing (LE Secure Connections) using the example provided by ST in the software tools example. I can sucessfuly complete the bluetooth pair using a Samsung A12, however if I use other smartphones like Google Pixel 6, Xiaomi 14T or even Huawei the pairing does not complete.
I have tried this with other manufacturers libraries and software and it works for all the smartphones. After inspecting the memory of the tag I found out they use a "Handover Select" record with an "Alternative Carrier" inside. I dont't know if this is why it is not working with other smartphones.
Could someone explain this better, and if so, how do I set this additional records?
Best regards.
Solved! Go to Solution.
2025-06-17 3:30 AM
You have the demo cycle code. Please adhere to rule 3 of https://debuggingrules.com/download-the-poster/
BR, Ulysses
2025-06-10 8:17 AM
Hi,
I guess this post is the continuation of https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/st25r3920b-for-oob-bluetooth-pairing/td-p/762600.
Please confirm that the pairing demo from the ST25 Embedded lib is the basis for your development and that ndefBluetoothLeInit (or ndefBluetoothSecureLeInit?) is being used instead of ndefBluetoothBrEdrInit and that the following mandatory AD are present in the pairing record:
| Value (1 byte) | Description |
| 0x1B | LE Bluetooth Device Address |
| 0x1C | LE Role |
Using an Handover select ('Hs') record in addition to the pairing record will not improve the compatibility with other phones.
The development team has recently found that the length of the LE oob record may be incorrect. A fix is available in ndef_type_bluetooth.c attached file.
With this fix, the following LE oob record can be built:
# Record #1: MIME type (RFC 2046) record:
Type Name Format: MIME type (RFC 2046)
Short Record
type: "application/vnd.bluetooth.le.oob"
Payload length: 26 bytes
Payload data:
[00] 08 1B 50 51 52 53 54 55 AA 02 1C 00 0D 09 53 54 |..PQRSTU......ST|
[10] 32 35 52 20 64 65 76 69 63 65 |25R device |
# NDEF message:
[00] D2 20 1A 61 70 70 6C 69 63 61 74 69 6F 6E 2F 76 |. .application/v|
[10] 6E 64 2E 62 6C 75 65 74 6F 6F 74 68 2E 6C 65 2E |nd.bluetooth.le.|
[20] 6F 6F 62 08 1B 50 51 52 53 54 55 AA 02 1C 00 0D |oob..PQRSTU.....|
[30] 09 53 54 32 35 52 20 64 65 76 69 63 65 |.ST25R device |
and the phone properly proposes to pair the device once the record has been read.
Let me know whether this fixes your issue.
Rgds
BT
2025-06-11 3:43 AM
Hello,
Yes this thread is the follow up of the post you have mentioned. I can show you the code that I am using to fill the BLE information:
int BLEHandler::SetOOBPairData(uint8_t *ndefBuf, uint16_t ndefBufSize)
{
pcomm::ble::BLEHandler& BLE = pcomm::ble::BLEHandler::Instance();
ndefTypeBluetooth bluetooth;
ndefRecord leOobRecord;
ndefType ndefBt;
ndefStatus rc;
static uint8_t tkBuf[BLE_TK_LEN];
if (ndefBuf == NULL)
return ERR_PARAM;
/* Reset bluetooth record */
rc = ndefBluetoothReset(&bluetooth);
if (rc != ERR_NONE)
return rc;
/* Get bluetooth informations - Address, Address Type, Random and Confirm value */
bt_le_oob_get_local(0, &oob_data);
/* EIR Field 1: LE Device Address: Mandatory - 6 LSB bytes: Device address, 7th byte: Address type (Public/Random) */
uint8_t eirLeAddress[9] = { 8, NDEF_BT_EIR_LE_DEVICE_ADDRESS };
memcpy(&eirLeAddress[2], oob_data.addr.a.val, 6);
eirLeAddress[8] = oob_data.addr.type;
/* EIR Field 2: LE Role: Mandatory */
uint8_t eirLeRole[3] = { 2, NDEF_BT_EIR_LE_ROLE, NDEF_BLE_ROLE_PERIPH_ONLY };
/* Generate random TK */
rc = BLE.GenerateRandomTK(tkBuf, BLE_TK_LEN);
if (rc != 0)
return rc;
/* EIR Field 3: Temporary Key (TK) for secure pairing */
uint8_t eirTk[18] = { 17, NDEF_BT_EIR_SECURITY_MANAGER_TK_VALUE };
memcpy(&eirTk[2], tkBuf, BLE_TK_LEN);
/* EIR Field 4: Confirmation Value - Needed for LE Secure Connections */
uint8_t eirSecureConnConfirmation[18] = { 17, NDEF_BT_EIR_LE_SECURE_CONN_CONFIRMATION_VALUE };
memcpy(&eirSecureConnConfirmation[2], oob_data.le_sc_data.c, BLE_SC_CONFIRMATION_VALUE_SIZE);
/* EIR Field 5: Randomizer Value - Needed for LE Secure Connections */
uint8_t eirSecureConnRandom[18] = { 17, NDEF_BT_EIR_LE_SECURE_CONN_RANDOM_VALUE };
memcpy(&eirSecureConnRandom[2], oob_data.le_sc_data.r, BLE_SC_RANDOM_VALUE_SIZE);
/* EIR Field 7: LE Flags: BR/EDR not supported */
uint8_t eirLeFlags[3] = { 2, NDEF_BT_EIR_FLAGS, 0x04 };
/* EIR Field 8: Device local name */
const char *localName = bt_get_name();
uint8_t eirLocalName[2 + strlen(localName)] = { (uint8_t)(1 + strlen(localName)), NDEF_BT_EIR_COMPLETE_LOCAL_NAME };
memcpy(&eirLocalName[2], localName, strlen(localName));
/* Set all EIR */
rc = ndefBluetoothSetEir(&bluetooth, (uint8_t *) &eirLeAddress);
if (rc != ERR_NONE)
return rc;
rc = ndefBluetoothSetEir(&bluetooth, (uint8_t *) &eirLeRole);
if (rc != ERR_NONE)
return rc;
rc = ndefBluetoothSetEir(&bluetooth, (uint8_t *) &eirTk);
if (rc != ERR_NONE)
return rc;
rc = ndefBluetoothSetEir(&bluetooth, (uint8_t *) &eirSecureConnConfirmation);
if (rc != ERR_NONE)
return rc;
rc = ndefBluetoothSetEir(&bluetooth, (uint8_t *) &eirSecureConnRandom);
if (rc != ERR_NONE)
return rc;
rc = ndefBluetoothSetEir(&bluetooth, (uint8_t *) &eirLeFlags);
if (rc != ERR_NONE)
return rc;
rc = ndefBluetoothSetEir(&bluetooth, (uint8_t *) &eirLocalName);
if (rc != ERR_NONE)
return rc;
/* Init BLE record */
rc = ndefBluetoothLeInit(&ndefBt, &bluetooth);
if (rc != ERR_NONE)
return rc;
rc = ndefTypeToRecord(&ndefBt, &leOobRecord);
if (rc != ERR_NONE)
return rc;
/* Encode the record starting after the first two bytes that are saved to store the NDEF file length */
ndefBuffer bufRecord = { &ndefBuf[2], (uint32_t)(ndefBufSize - 2) };
rc = ndefRecordEncode(&leOobRecord, &bufRecord);
if (rc != ERR_NONE)
return rc;
/* Store the NDEF file length on the two first bytes */
ndefBuf[0] = bufRecord.length >> 8;
ndefBuf[1] = bufRecord.length & 0xFF;
CCC_Log("NDEF size: %d\n", bufRecord.length);
CCC_Log("NDEF :%s\n", hex2Str(bufRecord.buffer, bufRecord.length));
return rc;
}This seems to work well for some phones (like the Samsung A12) where the pairing always occurs. However with other phones like Xiaomi or Huawei the pairing procedure is never triggered. This seems strange to me because with other manufacturer' example I was able to complete the pairing. I can also show you what the NDEF message of the above code looks like:
2025-06-11 5:24 AM
Hi,
Have you updated the ndef_type_bluetooth.c file with the one I've attached?
By the way, why do you pair for LE rather than BR/EDR? Note that Bluetooth Low Energy (LE) and Bluetooth Classic (BR/EDR) are two are distinct Bluetooth technologies designed for different use cases.
Are you sure those Xiaomi or Huawei phones support Bluetooth LE?
From your January post, it seems that Felica/NFC T3T technology is being used. Do you still use this technology?
Regarding your question about Handover select ('Hs') record, see section 4.3 of the Bluetooth® Secure Simple Pairing Using NFC Application Document.
When using LE OOB pairing, only LE Bluetooth Device Address and LE Role are mandatory. Can you try to populate only LeAddress, LeRole and LocalName?
Can you do a full scan of the tag using TagInfo android app and share with me the resulting text and xml files?
Rgds
BT
2025-06-11 6:57 AM
Hello,
Yes I have replaced that file with the one that you have sent me, however it seems that the only difference is in line 347:
/* For BR/EDR only, but no test needed because length is 0 in that case */
if (type->id == NDEF_TYPE_ID_BLUETOOTH_BREDR)
{
length += ndefData->bufDeviceAddress.length;
}I am using Bluetooth Low Energy because it is a requirement for the application I am developping. Additionaly, also LE Secure Connections (Level 4 of Security) is required, so the fields of Confirmation and Random values generated by the bluetooth stack are also required.
Yes Xiaomi 14T that I am currently using, is one of the most recent Xiaomi smartphones and so it supports Bluetooth Low Energy. The most weird thing to me is that it follows perfectly with Samsung A12 but with my Xiaomi it doesn't even trigger the procedure. However when I run this example from Nordic works on all smarphones. Nordic NFC Pair
Yes, actually the technology being used is T4T (Type 4 Tag), that comes from your example of card emulation for ST25R3920B, as this chip needs to be working as a tag in the moment of pairing.
For some reason, I am not able to read the ST25R3920B with the TagInfo application, it only works with NFC tools. However I can read nordic tag and show you the all the details. As theirs is working, maybe the information on that tag can help you understanding if something is missing.
2025-06-11 9:14 AM
Hi,
can you make sure that only T4T is emulated (set RFAL_FEATURE_NFCF to false in rfal_platform.h)? When using TagInfo, make sure to wait enough time to complete the reading. If this is still failing, can you set a breakpoint after demoEncodeBluetoothRecord and dump the memory content of ndefFile and share the memory content with me?
Can you provide information about Xiaomi or Huawei phone (model and Android version)?
The NDEF message from Nordic has an extra Tnep record ('Tp') that uses the well-known service name urn:nfc:sn:handover. Can you clone the Nordic NDEF message on a physical tag (or simply as the ndefFile content of the ST25R3920B emulated tag) and remove the Tnep record (of course the overall NDEF length needs to be reduced)? Still working with Xiaomi or Huawei phone? Make sure to double check the content of the NDEF with TagInfo or NFC tools. Can you remove the Handover select record and keep only the LE oob record? Still working with Xiaomi or Huawei phone?
Compared with your LE OOB record, the Nordic LE OOB record has an extra Appearance (0x19) field. this should not make a difference but can you try to add it?
Rgds
BT
2025-06-11 9:47 AM
Hello, I cannot disable the NFCF technology because the other part of my application needs it make data exchange with a smartphone application (in a P2P fashion). I really can't use the TagInfo application, no matter how long I want but I can dump the memory of NDEF file after the encode function:
NDEF size: 116
D220516170706C69636174696F6E2F766E642E626C7565746F6F74682E6C652E6F6F62081B8EA7995C2A6901021C0011107FEA09E3F1EB30BF1D080D88ADED7B4B11228E6E28862CA1E8937AB6CB2BC6E2C2D711235FBE39E671EAB8CCECD3E97CF76DFD710201040B094454785F4343435F444B
This should match the payload I have sent earlier in NFC Tools, plus the header information that should be also correct.
The Xiaomi phone is a Xiaomi 14T, Android 15; the Huawei is a P40-Lite I am not really sure about the android version of this one but I think its 10. The basepoint is that with nordic example they both work, so both should support BLE and OOB Pair. I dont́ think that cloning the tag will do much, as then the phone needs to interact with the board bluetooth stack in order to paitr.
I had already tried to "clone" the nordic information into my application bnut without success. However I was putting all in (the "tp" record included). I can try to add manually the rest of the information and see if it works.
2025-06-11 1:59 PM
Hi,
what is the value of the 2 first bytes of the ndefFile after the encode function (this should be the length of the NDEF message i.e. 00h 74h)?
"I dont́ think that cloning the tag will do much, as then the phone needs to interact " Well, the phone is supposed to display "do you want to pair with xxxx?" once the oob record has been read and before any other interactions. The goal is to check whether the phone reacts on the Tnep handover record or on the oob record or on Hs record + oob record.
"I cannot disable the NFCF technology because the other part of my application needs it make data exchange with a smartphone application (in a P2P fashion)". Do you mean that RFAL_NFC_POLL_TECH_AP2P and RFAL_NFC_LISTEN_TECH_AP2P are present in your discParam.techs2Find and that DEMO_CARD_EMULATION_ONLY has been removed? Can you share more details on the value of your discParam.techs2Find? If AP2P is configured in your application, some phones will enter into P2P and will not read the NDEF message. In order to debug your issue, please make sure to have only CE mode in NFCA. This will help to understand the pairing problem. And for sure when having only NFCA CE, TagInfo can read the card emulation.
Rgds
BT
2025-06-12 2:05 AM
Hello,
I think I haven't understand the first part of the reply. After the encode function we get a raw buffer as the one I have sent you. I can decode the payload for you:
D2h - Header - 5 LSB -> Flags (1101 0) - This means the bits of Message Begin, Message End and Short Record are set; TNF (010) - MIME Record Type;
20h - Type Length
51h - Payload Legth
61h to 62h - Type: application/vnd.bluetooth.le.oob
08h to end - Payload: Bluetooth data
For the tag clonation, I have tried to clone on the ST25R3920B while was in card emulation but did not work. In a normal passive tag, I was able to sucessfully clone the tag and it worked with all smartphones I currently have for test (Xiaomi, Huawei, Google and Samsung), the pairing prompt appeared on all of them.
As for my NFC technologies I have 2 distinct functions, one for the P2P data exchange with the smartphone and other for the card emulation and BLE Pairing. I will leave the code snippets here:
flags = RFAL_NFC_POLL_TECH_A | RFAL_NFC_LISTEN_TECH_A
int NFCHandler::PollTargets(int flags, uint32_t duration)
{
if (m_Initialized == false)
return -ENODEV;
if (flags == 0u)
return -EINVAL;
if (rfalNfcGetState() != RFAL_NFC_STATE_IDLE)
rfalNfcDeactivate(RFAL_NFC_DEACTIVATE_IDLE);
/* Retrieve default discovery parameters */
rfalNfcDefaultDiscParams(&m_discParam);
//m_discParam.notifyCb = m_fncPollNotification;
m_discParam.p2pNfcaPrio = true;
m_discParam.totalDuration = 1000;
m_discParam.techs2Find = flags;
m_discParam.wakeupEnabled = true;
m_discParam.wakeupConfigDefault = false;
/* Wake up mode configurations */
m_discParam.wakeupConfig.period = RFAL_WUM_PERIOD_500MS;
m_discParam.wakeupConfig.swTagDetect = false;
m_discParam.wakeupConfig.irqTout = false;
/* ST25R3920B does not support capacitive sensing */
m_discParam.wakeupConfig.cap.enabled = false;
m_discParam.wakeupConfig.indPha.enabled = false;
m_discParam.wakeupConfig.indAmp.enabled = true;
m_discParam.wakeupConfig.indAmp.autoAvg = true;
m_discParam.wakeupConfig.indAmp.delta = 50;
m_discParam.wakeupConfig.indAmp.aaWeight = RFAL_WUM_AA_WEIGHT_8;
m_discParam.wakeupConfig.indAmp.reference = 200;
m_discParam.wakeupConfig.cap.reference = RFAL_WUM_REFERENCE_AUTO;
m_discParam.wakeupConfig.indPha.reference = RFAL_WUM_REFERENCE_AUTO;
m_pollDuration = duration;
ReturnCode rc = rfalNfcDiscover(&m_discParam);
if (rc != ERR_NONE)
{
platformLog("rfalNfcDiscover, with ret=0x%x\n", (uint8_t) rc);
return -EBUSY;
}
rfalNfcWorker();
}
As for my card emulation function I got this:
int NFCHandler::InitCardEmulationMode(uint32_t duration)
{
int rc = 0;
k_thread_suspend(m_pollThreadId);
if (!m_Initialized)
return -ENODEV;
if (rfalNfcGetState() != RFAL_NFC_STATE_IDLE)
rfalNfcDeactivate(RFAL_NFC_DEACTIVATE_IDLE);
rfalNfcDefaultDiscParams(&m_discParam);
m_discParam.devLimit = 1U;
m_discParam.notifyCb = m_fncPollNotification;
m_discParam.totalDuration = 60000U;
m_discParam.techs2Find = RFAL_NFC_TECH_NONE;
#if RFAL_SUPPORT_CE && RFAL_FEATURE_LISTEN_MODE
memcpy( gNfcfNfcid, ceNFCF_nfcid2, RFAL_NFCF_NFCID2_LEN );
memcpy( ndefFile, (uint8_t *)demoNdefFile, demoNdefFileLen );
/* Update AIB Ln with actual NDEF length */
InformationBlock[12] = demoNdefFile[0];
InformationBlock[13] = demoNdefFile[1];
uint16_t checksum = 0;
for (int i = 0; i < 14; i++)
{
checksum += InformationBlock[i];
}
InformationBlock[14] = checksum >> 8;
InformationBlock[15] = checksum & 0xFF;
#if RFAL_SUPPORT_MODE_LISTEN_NFCA
/* Set configuration for NFC-A CE */
memcpy(m_discParam.lmConfigPA.SENS_RES, ceNFCA_SENS_RES, RFAL_LM_SENS_RES_LEN); /* Set SENS_RES / ATQA */
memcpy(m_discParam.lmConfigPA.nfcid, ceNFCA_NFCID, RFAL_LM_NFCID_LEN_04); /* Set NFCID / UID */
m_discParam.lmConfigPA.nfcidLen = RFAL_LM_NFCID_LEN_04; /* Set NFCID length to 7 bytes */
m_discParam.lmConfigPA.SEL_RES = ceNFCA_SEL_RES; /* Set SEL_RES / SAK */
m_discParam.techs2Find |= RFAL_NFC_LISTEN_TECH_A;
#endif /* RFAL_SUPPORT_MODE_LISTEN_NFCA */
#if RFAL_SUPPORT_MODE_LISTEN_NFCF
/* Set configuration for NFC-F CE */
memcpy(m_discParam.lmConfigPF.SC, ceNFCF_SC, RFAL_LM_SENSF_SC_LEN); /* Set System Code */
memcpy(&ceNFCF_SENSF_RES[RFAL_NFCF_CMD_LEN], ceNFCF_nfcid2, RFAL_NFCID2_LEN); /* Load NFCID2 on SENSF_RES */
memcpy(m_discParam.lmConfigPF.SENSF_RES, ceNFCF_SENSF_RES, RFAL_LM_SENSF_RES_LEN); /* Set SENSF_RES / Poll Response */
m_discParam.techs2Find |= RFAL_NFC_LISTEN_TECH_F;
#endif /* RFAL_SUPPORT_MODE_LISTEN_NFCF */
#endif /* RFAL_SUPPORT_CE && RFAL_FEATURE_LISTEN_MODE */
rc = rfalNfcDiscover(&m_discParam);
/* Start timeout timer */
k_timer_start(&m_cardEmulationTimer, K_SECONDS(duration), K_NO_WAIT);
k_thread_resume(m_cardEmulationThreadId);
return rc;
}Finally for my technologies defines:
#define RFAL_SUPPORT_MODE_POLL_NFCA true /*!< RFAL Poll NFCA mode support switch */
#define RFAL_SUPPORT_MODE_POLL_NFCB true /*!< RFAL Poll NFCB mode support switch */
#define RFAL_SUPPORT_MODE_POLL_NFCF true /*!< RFAL Poll NFCF mode support switch */
#define RFAL_SUPPORT_MODE_POLL_NFCV true /*!< RFAL Poll NFCV mode support switch */
#define RFAL_SUPPORT_MODE_POLL_ACTIVE_P2P true /*!< RFAL Poll AP2P mode support switch */
#define RFAL_SUPPORT_MODE_LISTEN_NFCA true /*!< RFAL Listen NFCA mode support switch */
#define RFAL_SUPPORT_MODE_LISTEN_NFCB false /*!< RFAL Listen NFCB mode support switch */
#define RFAL_SUPPORT_MODE_LISTEN_NFCF true /*!< RFAL Listen NFCF mode support switch */
#define RFAL_SUPPORT_MODE_LISTEN_ACTIVE_P2P true /*!< RFAL Listen AP2P mode support switch */
/*******************************************************************************/
/*! RFAL supported Card Emulation (CE) */
#define RFAL_SUPPORT_CE ( RFAL_SUPPORT_MODE_LISTEN_NFCA || RFAL_SUPPORT_MODE_LISTEN_NFCB || RFAL_SUPPORT_MODE_LISTEN_NFCF )
/*! RFAL supported Reader/Writer (RW) */
#define RFAL_SUPPORT_RW ( RFAL_SUPPORT_MODE_POLL_NFCA || RFAL_SUPPORT_MODE_POLL_NFCB || RFAL_SUPPORT_MODE_POLL_NFCF || RFAL_SUPPORT_MODE_POLL_NFCV )
/*! RFAL support for Active P2P (AP2P) */
#define RFAL_SUPPORT_AP2P ( RFAL_SUPPORT_MODE_POLL_ACTIVE_P2P || RFAL_SUPPORT_MODE_LISTEN_ACTIVE_P2
2025-06-12 3:17 AM
Hi,
"I think I haven't understand the first part of the reply. After the encode function we get a raw buffer as the one I have sent you. I can decode the payload for you". Well, I am used to decode NDEF records :-). The demoEncodeBluetoothRecord fills the ndefFile buffer. The 2 first bytes of this buffer are supposed to be the NDEF length. I just want to verify that this length is correct. The dump (D2 20 51 etc.) is basically the content of &ndefFile[2] whereas I want to see the full file i.e. &ndefFile[0] starting with the NDEF length.
"In a normal passive tag, I was able to successfully clone the tag and it worked with all smartphones": can you remove the Tnep Tp record: is it still working on all phones? can you remove the Handover Select Hs record: is it still working on all phones? Make sure to update the ndef length accordingly and to update the Message Begin/Message End in the record header.
"As for my NFC technologies I have 2 distinct functions, one for the P2P data exchange with the smartphone and other for the card emulation and BLE Pairing. I will leave the code snippets here".
Rgds
BT