ST25 NFC/RFID tags and readers

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STEVAL_SMARTAG1 Error to follow the quick start guide

I am having this problem with this product, as I could not compile the provided firmware successfully once I enable the UART printf. I am using the keil project. once I uncomment the UART printf . I got the following error:error Due to flash size c...

0690X000009Z5RYQA0.bmp
ADSB by Associate III
  • 556 Views
  • 1 replies
  • 0 kudos

Resolved! How to use UART interface instead of SPI with X-NUCLEO-NFC03A1 and X-CUBE-NFC3 polling demo

I have the X-NUCLEO-NFC03A1 expansion board connected to the NUCLEO-F401RE, successfully running the demo polling code from X-CUBE-NFC3. I would like to modify the code to allow the two boards to communicate using UART alone (no SPI pins necessary). ...

Resolved! NFC as wireless EEPROM memory

HELLO ALL! i want to do point to point (P2P) data exchange between the NFC and a smart phone,Im new to NFC, require 64Kbyte EEPROM and mcu can write it, how to choose the chip

Resolved! Cannot have access to writable memory or it's size (Android App). error :TAG_CMD_CALLED_FROM_UI_THREAD

I'm working on an android app and using your SDK (using version 1.5.1).The app can read the Tag name and UID, however, I have not been able to make it read the memory size or the content of the NDEF message.String tagName = mNfcTag.getName(); TextVie...

Eraqu by Associate
  • 814 Views
  • 2 replies
  • 0 kudos

Resolved! Listen Mode in X-Nucleo-NFC03A1

I have the X-Nucleo-NFC30A1 with the Cr95HF chip. My question is: Is the Listen Mode supported for Type A tags?I used the X-Cube-NFC3 v2.0.0 and managed to get the Tag Detector working. But I am trying to implement the Listen Mode and am facing probl...

Resolved! how to access the full freq version of the S/W ?

The Eval kit GUI allows to evaluate the ST25RU3993 whatever the regional settings/frequency are (840 - 960MHz). This wide-freq version seems to be reserved for evaluation purpose only while the standard version is freq limited (to match regional reg...

agnes by Associate II
  • 598 Views
  • 3 replies
  • 0 kudos

Resolved! The dynamic range of phase change in an RU3993

Hi,I am using one of the evaluation boards to test 3993. My objective is to determine the change in the phase of the reflected signal. For this reason, I use the movement detection mode that shows the Phase of the tag using the linear I & Q RSSI valu...

NKhal by Associate
  • 622 Views
  • 2 replies
  • 0 kudos