ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! In EVAL Kit of ST25RU3993, why do we give Buffer positive supply, internally regulated to Low Power DIfferential Power output (0 dBm )

In the schematic for EVAL Kit why we have used Inductors and why we have given Buffer positive supply, { internally regulated } to RF Output of both Internal Amplified and also for Low power Amplifier. PFA image attached.Secondly why they have used ...

0693W000008yctfQAA.png

Resolved! How I can increase the speed of the RFID Reader?

I'm using the ST25R3911 kit, to create code then read continuos information by ISO14443A protocol.I have another board ( SIC-4310) then send me continuos information, when I trying to read I lost some packages, for example, I send 64 bytes each packa...

GPaiv.1 by Associate III
  • 1461 Views
  • 9 replies
  • 0 kudos

Resolved! ST25R3911B-DISCO firmware supporting UART or I2C?

Hi,I have an ST25R3911B-DISCO and have discovered that UART and I2C are not supported on the loaded firmware through searching Google on how to use the interfaces.I am wondering if there have been any updates in the last two years on this subject.If ...

MMcAl.1 by Associate III
  • 705 Views
  • 1 replies
  • 0 kudos