When I look at source code I can only see bsp driver for ST25r95???It looks like it can detect tag of type ISO14443 or 15693 but the IDs read is not correct and sometimes it is and board reset randomly.My board is NUCLEO-L476RG.
Thanks Brian for the answer. I have ended up to same conclusion investigating a little bit more the source code and tesing a few modified firmware.Now I can read all Tag of type 14443A/B and 15693, firmware seems quite stable.I have going to start a ...
Looking more deeply in code and datasheet, both ST25r95 and CR95HF responds to the same chip ID "NFC FS2JAST4" to the IDN command 0x1.Looks like CR95HF has an additional UART interface availableST25r95 supports Card emulation (ISO/IEC 14443-3 Type ...