ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ST25R3911B or the ST25R3916?

I'm trying to decide between the ST25R3911B or the ST25R3916? I realize the ST25R3916 is newer; but newer does not always equal better. Are there any advantages to developing with the ST25R3911B? Primary purpose is to read 15683 transponders in a ...

Resolved! Input Power calculation

Hello. I use board st25ru3993-eval and application ST25RU3993 Reader Suite. When tags are readed we can see RSSI LOG Channel I & Q and Input Power. RSSI LOG Channel I & Q we can find in RSSI Display Register in AS3993, but i do not understand how cal...

0693W00000AMeM2QAL.jpg 0693W00000AMeXOQA1.png
DFomi.1 by Associate II
  • 942 Views
  • 4 replies
  • 0 kudos

Resolved! ST25R3911b vs CLRC663

Hi, I am not sure if this is the right place to ask this question.We are building a new product which requires NFC read/write support, we narrowed our options to one of 2 chips st25r39x and another nxp chip clrc663.Is there any advantage of using the...

mohamed2 by Associate II
  • 1340 Views
  • 3 replies
  • 0 kudos

Resolved! Nucleo NFC04 interrupt isn´t working

Hello,I´m using an STM32 Nucleo G474RE and an X-NUCLEO-NFC04A1 and I want to use the interrupt function of the NFC board to detect a changing field, but the interrupt doesn´t get triggered by using this code (based on a example from ST):#include "mai...

Kampi by Associate III
  • 4499 Views
  • 10 replies
  • 0 kudos

Resolved! st25R3911.dll complete SendReceive function

We are using your board ST25R3911B but we need to use this board by program in c/c++. We found your DLL demo, but is it possible to send only first command to comunicate with ISO14443 type A like RQA/ANTICOLL/SEL and not a send and receive generic, a...

asant.1 by Associate II
  • 1512 Views
  • 5 replies
  • 0 kudos

How optimize code in ST25R3911B-DISCO ?

Hi,I'm using ST25R3911B-DISCO for reading tags, but I'm interested in optimizing my code.When a search how optimizing codes in C, I see people using #pragma but I don't have the answer in my code after in the proprieties in STMcubeIDE I will go to op...

0693W00000AMY1IQAX.png
GPaiv.1 by Associate III
  • 1037 Views
  • 3 replies
  • 0 kudos

Resolved! HardFault_Handler() error in SPI

Hi, When I leave my code to play for more than one hour I received the error HardFault_Handler(), I found in registers whats the last line executed before entering in the error function, below I put a picture of this part of the code.  Note: That err...

0693W00000AMXbnQAH.png
GPaiv.1 by Associate III
  • 1618 Views
  • 7 replies
  • 0 kudos