Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

GitLab Projects

Good morning, I will try to be as concise as possible, I'm looking to change the location one of my GIT projects points to, I have a first software (STM32) where modifications have been made, and today I am looking to add a new project (STM32) to the...

Unable to generate a PWM pulse

I am using the ST discovery board, which has STM8S003K3. I have written a code that generates a PWM pulse when ADC senses that the input voltage is higher than a threshold value. I have tested this program with a Potentiometer and verified the wavefo...

STM32L476 IOExpander trouble turning on LEDS

Hello, I am writing some code to turn on an LED on my board through the IOExpander (STMPE811) but am facing some issues. I am able to read and write to I2C, and have done the following:written 1 to 0x10 (GPIO_SET_PIN) (Writing 1 to this bit causes th...

easy by Associate
  • 854 Views
  • 0 replies
  • 0 kudos

M95M02-DRMN6TP

M95M02-DRMN6TPMay I ask if there are any cases that cannot be   EEPROM programming   that can be shared?We are unable to  EEPROM programming,thank you

LINZIBIN by Associate II
  • 1738 Views
  • 3 replies
  • 0 kudos

M95P32: Missing RAM block in the Block diagram

Hi,Why is there no RAM block inside the Block diagram?In the document AN5747 (Page EEPROM memory architecture) there is a RAM block mentioned, but in the block diagram from the M95P32 datasheet no RAM block is available/visible.Thanks in advancenobod...

nobody_0-1719838574624.png
nobody by Associate II
  • 1615 Views
  • 2 replies
  • 0 kudos