Others: hardware and software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MB1419 - RC snubber design

Hey everyone!I am trying to understand the snubber design for a 3 phase inverter to reduce ringing. What is the difference between placing the RC snubber:- between each phase output and ground (3x RC snubber)- between drain and source of every mosfet...

jakub1 by Associate
  • 564 Views
  • 0 replies
  • 0 kudos

RS485 Communication disturb in run time

In one project we are using ST1480ABDR (Transceiver) and Baud rate is 115200. One master and 19 Slave connected in star topology. Please find attached reference termination resistor on both side, one at master and only one at slave. Run time our comm...

vrajesh by Associate II
  • 2260 Views
  • 6 replies
  • 3 kudos

Resolved! ULN2804A

Hello, I would like to knowto know, for the ULN2804A, if the logic gates invert or not.If so, is there an equivalence without inverting gates?

Elias1 by Associate II
  • 1565 Views
  • 5 replies
  • 2 kudos

Unable to download STSW-WPSTUDIO

Hello, I bought a STWLC38 evaluation board and I need to install STSW-WPSTUDIO for adjusting and configuring the board. While I'm trying to download the software, it shows error "This software is not available for download." Can somebody help me to e...

Capture.PNG

Need clarification on PCN

Will you please confirm on below part numbers that whether there will be any change in electrical parameters of the affected MPN depending on their PCN. For that do we need to verify any electrical parameters again?  Part TypePCN Tracking NoType of C...

Reading STUSB4500 USB PD status via I2C

The USB PD status register is a combination of 4 registers.The question is when read, are they interpreted as big endian or little endian?so 0x91 0x92 0x93 0x940x91 = bit 0-7, or 28 - 31?0x92 bit 8-110x93 ...0x94 ...The manual and programming guide a...

fbrown by Associate
  • 1015 Views
  • 1 replies
  • 0 kudos

STUSB4500 damaged during reconnection

Hi,We have a custom implementation based around STM32H7 and STM32F1.The application is powered internally by a rechargable 4s li-ion battery.We use USB-PD to charge the device, and USB 2.0 to communicate with the STM32H7 through an external ULPI-PHY....

STUSB4500-implementation.png
LFjær.1 by Associate
  • 1544 Views
  • 3 replies
  • 0 kudos