Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Suggestions for better blue pill performance

Hello,i am working for now on a diy project.In this project i am interfacing LoRa SX1278 (SPI), MPU6050 (I2C) and NEO-6M (UART) with the STM32F103C8 (blue pill).All in all it is working but because all this sensors and modules are served in the loop,...

hamo by Senior
  • 5042 Views
  • 10 replies
  • 3 kudos

Resolved! Unable to Programm Blue pill

When I try to program my Blue Pill over UART in the Stm32CubeProgrammer it give me this Error message:13:11:23 : Serial Port ttyUSB0 is successfully opened.13:11:23 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1,0,...

super_EEG by Associate II
  • 11134 Views
  • 15 replies
  • 3 kudos

Resolved! Debug Blue Pill with Stlink-V3minie

HI!I recently purchased some ST products, attempting to program and debug.I initially purchased a STM32 Blue Pill (STM32f103) along with a Mini St-Link V2 (Clone). Then I purchased an STM32F3VE board.I was able to program both boards using ST-LINKV2 ...

Resolved! STM32F103C8T6 (Blue Pill) CAN BUS Communication

Hi, I´m trying to communicate two blue pills between them using CAN bus, but when I try to run it, it doesn´t even finish the start up, because I tried to use a blink program selecting the CAN in the .ioc and not using it and doesn´t work.Does anyone...

Resolved! STM32 Blue Pill

HelloI came across with this board (STM32 Blue Pills) and instantly got many questions.1) I couldn't find it on CubeMX and could you please confirm that it is not present on CubeMX or it is just clumsy me?2) It seems that MPU is STM32F103xx which I b...

hashtala by Associate II
  • 8869 Views
  • 3 replies
  • 1 kudos

Resolved! STM32F103C8T6 Blue Pill USB Bootloader

Hello,I'm developing a USB bootloader for the STM32F103C8T6 Blue Pill (64KB / 128KB). I've seen many protocols and methods for doing this. Can you suggest the best method? I want to program the STM32F103C8T6 Blue Pill with STM Cube IDE software via U...

Resolved! Checking whether my Bluepill is real or fake?

I bought Bluepill devboards from two different sellers, paying extra to hopefully receive genuine STM chips. When I use the Bluepill Diagnostics Tool written by Terry Porter, the tool reports passing on all counts except for one:Declared flash not 65...

SSmit.5 by Associate
  • 8114 Views
  • 4 replies
  • 0 kudos

STM8AF528 flashing issue

Hi there,If I am flashing the .s19 file using st visual programmer I have observed that there is a flash memory corruption. But If I am flashing this with visual developer I am not facing any issue.Can anyone tell me is there any alternate SW tool fo...

vignesh_st3_0-1745411639058.png