Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM8AF5288 halt() supply current

Hi, I use a PCB that is reduced to one STM8AF5288 and 3 100nF Capacitors. No other components, all are removed. I supply it with 3,3V. I want to reduce current consumption in halt-mode to 4,5uA. Some others posted simliar problems, I could never find...

HolgerG by Associate
  • 1521 Views
  • 2 replies
  • 0 kudos

Resolved! TDA7265 not working in my Power amp project

For this project I used a TDA7265 in beige configuration directly following the circuit diagram from the datasheet. In testing, no sound is coming from the speaker, only a hum. I’m using a 12V 1 A dual rail supply with an 8 ohms speaker. I have demon...

image.jpg

Resolved! FPAS Declaration

Please kindly support to provide PFAS Declaration of MPN : M24C02-FMN6TP? Please kindly help to reply into my mail at RWIMINTO@OSIELECTRONICS.COMThank you.