Other: hardware

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Configuring ST10R168 UARTS

Posted on June 17, 2014 at 19:20What reload codes are used to configure the UART(s) on the ST10R167 to: 19200 38400 57600 Can a UART have a different baud rate on channel a and channel B (i.e. 38400 on Chan A and 57600 on chan B

Programming SDK

Posted on June 15, 2014 at 16:30Hi all, i found a ST72F321AR6T6 in my broken Driving Force GT. I have the control board with some buttons and a DC motor. I wanted to change the program inside the ST72F321AR6T6. How can i program the ST72F321AR6T6? I...

dnviti by Associate
  • 341 Views
  • 0 replies
  • 0 kudos

STR912 Partiry bit set Error.

Posted on April 09, 2014 at 13:48hi.dear i use to IAR compiler, default_form_lib_2.1_iar_5.30 library and jlink. it is my developer environment.  my chip is STR912FAW44. first. i initialize UART2 set None parity bit. second. i change to UART2 set  ...

ikassma by Senior
  • 402 Views
  • 3 replies
  • 0 kudos

UDP on SPEAr320S

Posted on May 22, 2014 at 16:38Hello, I need to know if the User Datagram Protocol is supported by the SPEAr320S and if there is a ''ready to use'' library to implement and use it. I also need the same informations about the TCP Protocol on the same...

g2399 by Associate
  • 286 Views
  • 0 replies
  • 0 kudos

Controlling PSD I/O-pins on uPSD3354 uC

Posted on May 15, 2014 at 11:18Hi, We need to modify one of our existing company products to be able to be controller by external I/O. The only externally available I/O-signals are the 6 JTAG pins. These JTAG pins are connected to the PLD I/O-Port C...

henk2 by Associate II
  • 349 Views
  • 0 replies
  • 0 kudos

Trying to find ST9 Visual Programmer for EPB

Posted on May 07, 2014 at 23:04Hello, I have an ST92f150-EPB the software installation CD is long gone, and I need to use my programmer. I have been serching for an STVP that will work with my programmer and my ST92F150JDV1QC chips but I can not fin...

spechin by Associate
  • 533 Views
  • 2 replies
  • 0 kudos

STR711FR2 USB Virtual Com Port IAR *HELP* needed.

Posted on April 08, 2014 at 14:00Hi,I have been looking at implementing USB VCP on a STR711FR2. I have downloaded the str71x demos from ST. I have built the project and got it running but when I plug into the USB port I get �Unknown Device� The boar...