Other: hardware

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using Virtual Com port driver on Win7 32/64 bits

Posted on December 05, 2012 at 20:31I am trying to use driver for MCBSTR9.inf thats working well on WinXP for a virtual com solutions, but in win7 i had many problems with the connection and could not send commands to microcontroller or receive from...

rafael by Associate
  • 321 Views
  • 2 replies
  • 0 kudos

STR911 spi master transmit problem

Posted on December 29, 2014 at 23:24Hi,I am using STR911FAW44X6 as SPI master to send out a hugh amount of data(136*256 bytes) to a SPI slave.  I set up CLK as 10MHz, CPHA=0, CPOL=0. The way I send out the data is as follows:            for ( j = 0;...

jian by Associate
  • 304 Views
  • 0 replies
  • 0 kudos

''C'' Library for ATmega8 and ST7590 Modem PLC

Posted on December 07, 2015 at 20:15For a project in prototype assembly stage it is necessary to link an 8-bit microcontroller with the modem ST7590T, for it would be desirable to have the ''C'' library that is mentioned in the 1076 User Manual (UM1...

C Library for ATmega8 to drive ST7590

Posted on December 07, 2015 at 20:10For a project in prototype assembly stage it is necessary to link an 8-bit microcontroller (ATmega8) with the modem ST7590T, for it would be desirable to have the ''C'' library that is mentioned in the 1076 User M...

M41T00S RTC reference schematics

Posted on October 26, 2015 at 07:18I am currently using STM32 to communicate with RTC chip M41T00SMF6, does anyone has a reference schematics for M41T00S ? Thanks.

ST7580 Modem UART Package CRC-32 Calculation Error

Posted on October 16, 2015 at 10:35Dear All,I tried to implement my own protocol for PLC modem with another company MCU. But When I calculate CRC32, it returns 32bir diffrent CRC and ST7580 ignore my package.For example;02 09 50 04 01 23 45 67 89 AB...

oner by Associate
  • 536 Views
  • 1 replies
  • 0 kudos