Other: hardware

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Secure Debug Authentication

Posted on October 17, 2014 at 15:19I am using SPEAr1310 (SPEAR1310CPUC evaluation board, revision 1). I want to use Memory Mapped debug interface to setup breakpoints. I have read the interface base address using cp14 Cooprocessor (DBGDRAR, DBGDSAR)...

vln by Associate
  • 302 Views
  • 0 replies
  • 0 kudos

Web Sockets

Posted on October 14, 2014 at 01:58I just bought a SPWF01SC.21  2.4 GHz IEEE 802.11 b/g/n transceiver module with a STM32 ARM Cortex-M3.I am new to ST processors, which IDE can I use to program it (does MBED work?) and does anyone have an example pr...

STR9 - Inrush current on the VDD supply

Posted on July 29, 2014 at 16:52Hi, I have a issue with the power supplies of my electronic board at start up of microcontroller STR912FAW47. Someone know the inrush current of microcontroller on VDD (1,8V) and VDDQ (3.3V) at power on? With an oscil...

jtual by Associate II
  • 351 Views
  • 2 replies
  • 0 kudos

Booting Linux or U-Boot via USB boot on SPEAr320

Posted on April 26, 2013 at 09:15Hello Is it  possible to boot Linux Kernel via the  USB boot mechanism in the SPAEr320 CPU? If yes, what tools are available to generate an image for a bootable USB stick? I hope to get at least a link to an approbri...

hj by Associate II
  • 571 Views
  • 2 replies
  • 0 kudos

STHV748 Capacitor size

Posted on September 01, 2014 at 09:34What is the range of capacitor sizes recommended to AC couple the substrate (exposed paddle) to ground? A 0.22uF is shown in the Application Note AN3961. Is there a limit on maximum size? Can the substrate be con...

nstc001 by Associate
  • 288 Views
  • 1 replies
  • 0 kudos

STHV748 anti-memory effect

Posted on June 18, 2014 at 12:05what is the anti-memory effect circuit and how does it benefit performance in case of 3-level/CW configuration? #ultrasound

nstc001 by Associate
  • 334 Views
  • 1 replies
  • 0 kudos

RF IPD for Internet of Things

Posted on September 05, 2014 at 11:11New compactness enabling Internet of Things to run overThe Internet of Things, a network of physical objects that contain embedded technology to sense, communicate and interact with their external environment is ...

VDDA connection for STR73x

Posted on August 01, 2014 at 15:39There are a few threads here about the possibility of VDDA connection to another source than the VDD does. In some of the ST technical notes about ADC, it is said that this really depends on the specific models. Som...

wxu8 by Associate
  • 268 Views
  • 0 replies
  • 0 kudos