Is the STLED524 still working correctly even if less then 120 LEDs are connected?
I want to know if i can use the STLED524 with 64 LEDs or is the device just working when all 120 LEDs are connected.
I want to know if i can use the STLED524 with 64 LEDs or is the device just working when all 120 LEDs are connected.
I have configured One way authentication mode and able to connect to the server successfully.After getting socket ID, I am using AT+SOCKW command to POST and GET.e.g. AT+SOCKW=00, 18<CR> (18 length is example)POST /api/Frames HTTP/1.1<CR><LF>DATA......
Hello,we are using STR73x for our application.We developed our own CAN boot loader that can download our application code to the flash and reboot the system. The reboot works fine.But we decided to change the application codes such that it does not...
Hello,How to programme this MCU? What tool can use? Ic no ST10F273-CEA
Lightning surge protection level should meet the standard:IEC61000-4-5Common mode:2kV, normal mode:1kVMalfunction:Level3Destruction :Level 1Mainly concerned on the PoE PD part and the Antenna part
Hi, I want to use the IDW01M1 under Arduino IDE because I already have the code to scan an UID of an NFC on this IDE and I want to send it with an http request but I can't use the IDW01M1 under Arduino IDE
4031407HERMAOE227EJMLT22009VQ947WVVPic attached We need to locate more stock ASAP
2M2i is a discontinued product?If there is a discontinued product, what is the substitute product?