Hi, I'm using EEPROM M95080. It is mentioned that the IC will send data at the falling edge. But its not happening exactly at the falling edge(there is a delay of almost 0.2 microseconds after the falling edge).
1)The IC supports both the modes of SPI(CPOL =1,CPHA =1 and CPOL =0,CPHA =0). On the master side I have configured the SPI with CPOL = 1and CPHA = 1.2) According to this master SPI mode the master will receive data at the rising edge and the slave se...