Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! st62t65c6 read and write data

Hi, we want to read and write data to st62t65c6 chip. I looked for a topic here and found one answer which suggests us to get an ST6-EPB but we can not find it anywhere. Is there any other way to achieve this? Regards

MKılı.1 by Associate II
  • 2348 Views
  • 1 replies
  • 0 kudos

STA8090WG driver for Intel Apollo lake

Hello Guys,   Did you have release STA8090WG driver that for discrete GNSS on Intel Apollo lake deticate UART ?   In our design, STA8090WG cannot transit NMEA data to the deticate UART, but can transit to an USB-to-UART dongle.   Is that the driver i...

Angus0723 by Associate II
  • 2573 Views
  • 3 replies
  • 0 kudos

HDMI ESD(?) IC Identification

Hello! I am trying to identify an IC that is connected to an Xbox One X's HDMI 2.1 output.The markings on the chip appear as:(ST logo)NFD (1st Line)741 (2nd Line)There are 18 solder balls attached to the pcb from the chip, arranged as so (after remov...

0690X000008wDMCQA2.jpg
GOetj by Associate
  • 3305 Views
  • 3 replies
  • 1 kudos

STM8L151G4 programming

I am using STVP and ST-Link V2 to program my STM8L151G4. I managed to upload my program once, but now I am not able to upload another one. It's one-file project, I build it using Small Device C Compiler. It gives me a .ihx file, which then I upload t...

Hydra by Associate
  • 1655 Views
  • 0 replies
  • 0 kudos

STUSB4500, sending command messages to source

HelloI have tried using the send command functionality on the I2C interface of the STUSB4500to issue various command messages to the source,in an attempt to poll information from an attached source.My code uses a slightly modified version of the Send...

C64_II by Associate
  • 918 Views
  • 0 replies
  • 0 kudos

ST Micro part from marking code

Posted on December 13, 2017 at 15:17I am trying to find ST micro part from marking code given on it. I am sure its a MOSFET or Transistor. Code is as below -First line: 130 082Second line: GK088 VUThird line: CHN 618Can someone help me to recognize ...

STHS34PF80 sensitivity

We are designing a led light with intrusion and occupancy feature. we found that STHS34PF80 will suit this application  but still we have some doubts about sensitivity with out changing the default gain setting.1.Do the sensitivity and performance ge...