Microcontrollers

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Why program loop in the function of irqSysHalt() ?

Hi, The program has been in irqSysHalt at the time of clock initialization, the clock initialization failed, but I don't know why? Has anyone encountered a similar problem?Program clock init fail:​The figure below is the clock configuration:​

Resolved! How to get double wire CAN from SPC5?

SPC5Studio asks for a TX and RX pin. I selected CAN 1 TX and RX pins and connected them to CAN 2 RX and TX pins I chose (I tried all manner of connections). I am trying to get CAN 2 to send a message. On the output I see a 0 to 5 V signal instead of ...

PSing.5 by Associate II
  • 294 Views
  • 1 replies
  • 0 kudos

How to choose CAN driver?

I enabled CAN 2 in low level drivers, chose the correct pins under pinout but I get error (undeclared variable) when I try to can_lld_start(&CAND2, &can_config_cfg0); How do I use a specific CAN bus in code and how do I enable it? Do I type &CAND5 fo...

PSing.5 by Associate II
  • 294 Views
  • 2 replies
  • 1 kudos

No activity on the CAN pins SPC560D discovery

I've written up plenty of programs prior and went on to developing a board from the 32 series and came back and since the can pins on the 56D device dont do anything.I've done a few programs already and have quick test programs to check but they all ...

AndreasPA by Associate III
  • 933 Views
  • 5 replies
  • 0 kudos

Resolved! How to get started with SPC5 ?

Hi everyone !I would like to learn about the SPC5 MCUs and do some example projects but I have found very little information/tutorials on the web.What would be a good place to start with ? Where can I find some good ressources ?Thank you very much

CBeau.2 by Associate
  • 463 Views
  • 2 replies
  • 0 kudos

Comunication interfaces for SPC58NG-DISP

Hi,I saw the user manual of the SPC58NG-DISP, in particular is the document called UM2255, and I have a doubt about the communication interface module shown. (image attach)I'd like to know if it is possible to have 2 CAN for this board.Where can I fi...

RD'Ig by Associate II
  • 548 Views
  • 2 replies
  • 0 kudos