I've written up plenty of programs prior and went on to developing a board from the 32 series and came back and since the can pins on the 56D device dont do anything.I've done a few programs already and have quick test programs to check but they all ...
Hey Team,Following the examples online , the wildcard range prevents me from inputting 0-120.I've also tried doing 0,120. that lets me input the value , generate the code but not actually show up on the screen
Hello,Doing some work using sd cards, and noticed that if i were to use the main.h file and have all my fatfs.h declared all the structs like FATFS / FIL / FRESULT spit out errors that theyre undefiend when cntrl clicking takes me to the file.unknown...
Hey all,for a can project im trying to enable the external clock, ticking the bypass oscillator box in my clock settings results in an inexpected reset.i've tried a few combinations and have spent a few hours on it and havnt managed to get it working...
Hello all.I'm playing around with the PIT interrupts and im finding that after setting up 3 seperate timers with different interrupt rates with the same priority setup in the IRQ Component rla. It's only constantly interrupting the PIT with the lowe...
More hands on videos with the stm32MP1, currently some of the startup material doesnt run smoothly or you have to make little changes to the commands etc etc.otherwise really we're better off going to something like begalbone. if it's a pain in the *...
No go unfortuantly , it would strange if that was the reason since it's been working fine until recently. (reference i turned off the OBE and set both pins to pull up)